CodeWarrior for MCU V10.6 Update 3.0.0 available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior for MCU V10.6 Update 3.0.0 available

CodeWarrior for MCU V10.6 Update 3.0.0 available

Greetings,

The third update for CodeWarrior for MCU V10.6 is available. This update includes the previous 1.0.0 and 2.0.0 updates, and applies to CodeWarrior for MCU v10.6 only.


New device support:

•             S12Z: S12ZVC96, S12ZVCA128, S12ZVCA192, S12ZVCA64, S12ZVCA96

•             DSC: MWCT1012, MWCT1212, MWCT1111

Updated support for silicon revisions:

•             Kinetis K Series: K11DN512A,  K11DX128A, K11DX256A, K21DN512A, K21DX128A, K21DX256A, K21FN1M0A, K21FX512A

See attached release notes for further details.

 

There are two ways of installation: Offline or Online. Offline installation is recommended as the size of the installation files is up to 900 MB (depending on the installed architectures).

 

Offline Installation:

  • Go to https://www.freescale.com/cwmcu10
  • Click on the 'Downloads' tab and select the product download:
    18925_18925.pngpastedImage_1.png
  • Select 10.6:
    18935_18935.pngpastedImage_2.png
  • Download the Update 3:
    18936_18936.pngpastedImage_3.png
  • From CodeWarrior for MCU10.6, select the menu Help > Install new Software and select the downloaded archive file:
    18937_18937.pngpastedImage_5.png
  • Check the MCU 10.6 Updates and go through the installation with 'Next >' button.
  • Restart Eclipse as prompted.

 

Online Installation

 

Full release notes are attached to this document.

标签 (1)
附件
无评分
版本历史
最后更新:
‎01-21-2015 03:22 AM
更新人: