CodeWarrior 11.1 编译的I2C模块代码有缺陷

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 11.1 编译的I2C模块代码有缺陷

666 Views
813270556
Contributor I

概述:使用MC9S12ZVL96MLF芯片与MPQ4262芯片进行I2C通信,MCU只能够对4262进行写操作,无法进行读操作。

过程分析:相同代码(I2C模块使用的了自动代码)使用 CodeWarrior 11.1的编译结果,MCU只能够对4262进行写操作,无法进行读操作。进行读操作时发现时钟与数据线被拉低无法释放。

使用CodeWarrior 10.7的编译结果 MCU 可以对4262进行读操作以及写操作。

问题:CodeWarrior 11.1版本与CodeWarrior 10.7版本的编译器存在哪些差异,导致编译结果存在缺陷。

0 Kudos
Reply
1 Reply

641 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 813270556 

Please refer answer in this thread

https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-11-1-%E7%BC%96%E8%AF%91%E7%9A%84I2C%E6%...

Thanks,

Jun Zhang

 

0 Kudos
Reply