CodeWarrior 10.6 exporting/importing project to arbitrary location. What is the simplest way pass the include directories paths when exporting so all the files don't have to be linked over again when the project is imported?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior 10.6 exporting/importing project to arbitrary location. What is the simplest way pass the include directories paths when exporting so all the files don't have to be linked over again when the project is imported?

2,951 次查看
rhana
Contributor III

IDE: CodeWarrior 10.6

 

Hello,

 

I am looking for a better solution to this problem. What I have done is exported project as a zip file. The project contained absolute paths to the location of my source and header files. After deleting the project completely from the hard disk, I unzip the project file in some other location then import the project once again (not to workspace.)

 

Going to Project --> C/C++ General

Next expand this category

Click on paths and symbols

 

in the "includes" tab, beneath languages select c,C,cc,cxx,cpp.

Paths to the include directories can be found here.

 

${ProjDirPath}\..\..\..\..\MyDirectory\mySubDirectory

 

Every time I import a project the links are broken.

 

How would I export the project with absolute paths, so that the exported project will have the correct relative paths in an arbitrary location on another workstation?

Is this broken or am I doing something wrong? Should I change the project to relative links before exporting?

 

I would like all of the required source and header files in the zipped project folder and for the project to be able to find

the files without someone having to specify their locations. Is there a tool for this?

 

 

I have browsed the forums for this already:

When exporting a project from CW 10.5 and then importing it On Another Computer, I get errors for lo...

Which would be the better way to export a codewarrior project and import in another PC?

 

Thank you.

标签 (1)
3 回复数

2,143 次查看
cesarrabak
Contributor III

Robert,

What do you mean with:

I unzip the project file in some other location then import the project once again (not to workspace.)

Which links exactly are the broken ones?

What header files are not found the system or yours?

--

Cesar Rabak

2,143 次查看
rhana
Contributor III

Ok, I followed your advice (thanks!). And the solution seems to be this:

Set all of the project paths to relative when exporting because all paths (abosute and relative) are preserved when exporting.

There are 2 parts to this process

Part #1:

In the Linked resources:

Right click project -> go to "Edit linked resource locations"

Click on the Linked Resources tab.

For all the resources that have been linked (there should be none missing here, denoted by the red circle and X) resolve by referencing them to their absolute location. Once this has been done for all the files click on the "Convert" button, which will convert them to locations with respect to the project location; provided the files have been added to the project correctly.

Part #2

Going to Project --> C/C++ General

Next expand this category

Click on paths and symbols

in the "includes" tab, beneath languages select c,C,cc,cxx,cpp.

Paths to the include directories can be found here.

All of these paths should be relative to your project.. this means..  "$ {ProjDirPath}\ "

How to do this: Click on the add button, click on the "variables" button, click on "ProjDirPath", click ok, then edit the field to include

the directory that contains the file for your project. (All of the source files and header files should be in your project directory.)

After having done this, export the project to a zip file.

I have tested this only importing after unzipping the project (not to work space) but it shouldn't make a difference.

There should not be any broken links when importing to an arbitrary location on your disk.

0 项奖励
回复

2,143 次查看
cesarrabak
Contributor III

Glad I've been helpful, Robert.

--

Cesar Rabak

0 项奖励
回复