Code Warrior 10.5.1 for PA - Install New Software not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior 10.5.1 for PA - Install New Software not working

ソリューションへジャンプ
15,244件の閲覧回数
PaulWalker
Contributor IV

I have Code Warrior for PA 10.5.1 installed and I am trying to add QCVS (for RCW work). The installation was done as a clean new install.

When I try to use Install New Software I get errors.

Please help.

Also, links to any offline install packages do not work for me (they send me back to the NXP Code Warrior main page).

FYI - if I try to navigate to any of the update locations in a web browser I get 'Page Not Found'.

The generated error is:

Some sites could not be found. See the error log for more detail. Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.pkt_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.buildtools_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.updatesite_win/content.xml. Remote host closed connection during handshake

0 件の賞賛
返信
1 解決策
15,211件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I have transcended QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5 to you, please pay attention to your email box to download it.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive"

元の投稿で解決策を見る

0 件の賞賛
返信
15 返答(返信)
316件の閲覧回数
petes1
Contributor II

I was able to get this working by modifying where the installation new software tool gets the new software, since it's still pointing to the old freescale.com address. If you go to help -> install new software... then click on the "available Software Sites" then update some of the locations to nxp from freescale, including the QCVS you should be able to get the tool. 

petes1_3-1758000269386.png

 

petes1_2-1758000206672.png

 

petes1_1-1758000123163.png

 

 

0 件の賞賛
返信
314件の閲覧回数
Priyaa
Contributor I

Still I was not able to get the tool

Getting error as below

image.png

0 件の賞賛
返信
8,567件の閲覧回数
lana0
Contributor I

I've used the link

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6529687&dkey=9017647

But it would not work for you.

 

You should:

0. log in to nxp

1. Open ticket support

2. Get a link from support

3. Support->Click on ticker <xxxxxx> -> Click on download, approve commitment and then goto next protal:

i.e. the link something as above.

it will be valid for a few days.

 

0 件の賞賛
返信
10,972件の閲覧回数
petes1
Contributor II

How can I get a copy of this, those sites are still down.... 

0 件の賞賛
返信
11,171件の閲覧回数
lana0
Contributor I

Can you send the offline install file to me, Thanks a lot!

0 件の賞賛
返信
15,199件の閲覧回数
PaulWalker
Contributor IV

I've got a bit further with this.

The Install New Software not working was because CodeWarrior installer still sets the download site as the old 'freescale.com'. I have edited and replaced with 'cache.nxp.com'. This information was very difficult to find! The QCVS installer now runs but generates MD5 hash errors (see attached). This also happens when running any of the update sites (build tools, eclipse, etc.). It also does the same in other versions of CodeWarrior (we also have v10.3). How do I sort this out?

0 件の賞賛
返信
15,205件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could download QCVS for Power Architectures Rev 4.5 from NXP public Web site.

Please login "www.nxp.com", then download the installation file from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->QorIQ Configuration and Validation Enablement Suite-> 4.5 QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive".

Then reopen CodeWarrior IDE, create a QCVS PBL project from "File->New->QorIQ Configuration Project", please enter "Project name" and select the processor to be used, click Next. Then in "Toolset selection" panel, please select "PBL - Preboot Loader RCW configuration"

13,365件の閲覧回数
debduttabanerje
Contributor III

I actually found the QCVS for PA 4.5 here and successfully added to codewarior-10.5.1.

Attached a screenshot of the location. It may useful for others.

0 件の賞賛
返信
15,202件の閲覧回数
PaulWalker
Contributor IV

Hi, Thanks for the answer. QoriQ Configuration and Validation Suite doesn't appear in my NXP software list. Also does not appear under the Code Warrior list. See screenshots attached. I am currently using an evaluation copy of Code Warrior 10.5.1. We have a licensed copy of Code Warrior 10.3 but have not upgraded yet. The online docs for Code Warrior says QCVS is free (unlicensed) so I wanted to try out and start looking at PBL/RCW configuration for our QoriQ T-series based boards. How do I get QCVS in my Code Warrior? Thanks again.

 

0 件の賞賛
返信
15,212件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I have transcended QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5 to you, please pay attention to your email box to download it.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive"

0 件の賞賛
返信
365件の閲覧回数
Priyaa
Contributor I
Hi, Can you send the QCVS offline installation packages to me

Thank you
0 件の賞賛
返信
11,166件の閲覧回数
lana0
Contributor I

Can you send the offline install file to me, Thanks a lot! Also

0 件の賞賛
返信
12,869件の閲覧回数
pipi95
Contributor I

Can you send the offline install file to me, Thanks a lot!

0 件の賞賛
返信
12,782件の閲覧回数
pipi95
Contributor I
I have already got one, Thanks a lot!
0 件の賞賛
返信
15,150件の閲覧回数
PaulWalker
Contributor IV

Hi,

Thanks for the offline install file. I have this installed and working now with Code Warrior 10.5.1.

Note I needed to de-select the option "Contact all update sites during install to find required software", else the install would fail with an error.

Thanks again

0 件の賞賛
返信