Code Warrior 10.5.1 for PA - Install New Software not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code Warrior 10.5.1 for PA - Install New Software not working

跳至解决方案
15,520 次查看
PaulWalker
Contributor IV

I have Code Warrior for PA 10.5.1 installed and I am trying to add QCVS (for RCW work). The installation was done as a clean new install.

When I try to use Install New Software I get errors.

Please help.

Also, links to any offline install packages do not work for me (they send me back to the NXP Code Warrior main page).

FYI - if I try to navigate to any of the update locations in a web browser I get 'Page Not Found'.

The generated error is:

Some sites could not be found. See the error log for more detail. Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.pkt_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.buildtools_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.updatesite_win/content.xml. Remote host closed connection during handshake

0 项奖励
回复
1 解答
15,487 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I have transcended QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5 to you, please pay attention to your email box to download it.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive"

在原帖中查看解决方案

0 项奖励
回复
15 回复数
592 次查看
petes1
Contributor II

I was able to get this working by modifying where the installation new software tool gets the new software, since it's still pointing to the old freescale.com address. If you go to help -> install new software... then click on the "available Software Sites" then update some of the locations to nxp from freescale, including the QCVS you should be able to get the tool. 

petes1_3-1758000269386.png

 

petes1_2-1758000206672.png

 

petes1_1-1758000123163.png

 

 

0 项奖励
回复
590 次查看
Priyaa
Contributor I

Still I was not able to get the tool

Getting error as below

image.png

0 项奖励
回复
8,843 次查看
lana0
Contributor I

I've used the link

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6529687&dkey=9017647

But it would not work for you.

 

You should:

0. log in to nxp

1. Open ticket support

2. Get a link from support

3. Support->Click on ticker <xxxxxx> -> Click on download, approve commitment and then goto next protal:

i.e. the link something as above.

it will be valid for a few days.

 

0 项奖励
回复
11,248 次查看
petes1
Contributor II

How can I get a copy of this, those sites are still down.... 

0 项奖励
回复
11,447 次查看
lana0
Contributor I

Can you send the offline install file to me, Thanks a lot!

0 项奖励
回复
15,475 次查看
PaulWalker
Contributor IV

I've got a bit further with this.

The Install New Software not working was because CodeWarrior installer still sets the download site as the old 'freescale.com'. I have edited and replaced with 'cache.nxp.com'. This information was very difficult to find! The QCVS installer now runs but generates MD5 hash errors (see attached). This also happens when running any of the update sites (build tools, eclipse, etc.). It also does the same in other versions of CodeWarrior (we also have v10.3). How do I sort this out?

0 项奖励
回复
15,481 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You could download QCVS for Power Architectures Rev 4.5 from NXP public Web site.

Please login "www.nxp.com", then download the installation file from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->QorIQ Configuration and Validation Enablement Suite-> 4.5 QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive".

Then reopen CodeWarrior IDE, create a QCVS PBL project from "File->New->QorIQ Configuration Project", please enter "Project name" and select the processor to be used, click Next. Then in "Toolset selection" panel, please select "PBL - Preboot Loader RCW configuration"

13,641 次查看
debduttabanerje
Contributor III

I actually found the QCVS for PA 4.5 here and successfully added to codewarior-10.5.1.

Attached a screenshot of the location. It may useful for others.

0 项奖励
回复
15,478 次查看
PaulWalker
Contributor IV

Hi, Thanks for the answer. QoriQ Configuration and Validation Suite doesn't appear in my NXP software list. Also does not appear under the Code Warrior list. See screenshots attached. I am currently using an evaluation copy of Code Warrior 10.5.1. We have a licensed copy of Code Warrior 10.3 but have not upgraded yet. The online docs for Code Warrior says QCVS is free (unlicensed) so I wanted to try out and start looking at PBL/RCW configuration for our QoriQ T-series based boards. How do I get QCVS in my Code Warrior? Thanks again.

 

0 项奖励
回复
15,488 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I have transcended QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5 to you, please pay attention to your email box to download it.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive"

0 项奖励
回复
641 次查看
Priyaa
Contributor I
Hi, Can you send the QCVS offline installation packages to me

Thank you
0 项奖励
回复
11,442 次查看
lana0
Contributor I

Can you send the offline install file to me, Thanks a lot! Also

0 项奖励
回复
13,145 次查看
pipi95
Contributor I

Can you send the offline install file to me, Thanks a lot!

0 项奖励
回复
13,058 次查看
pipi95
Contributor I
I have already got one, Thanks a lot!
0 项奖励
回复
15,426 次查看
PaulWalker
Contributor IV

Hi,

Thanks for the offline install file. I have this installed and working now with Code Warrior 10.5.1.

Note I needed to de-select the option "Contact all update sites during install to find required software", else the install would fail with an error.

Thanks again

0 项奖励
回复