Cant find hidef.h in CW5.1 when compiling NCV7383EVB_firmware.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cant find hidef.h in CW5.1 when compiling NCV7383EVB_firmware.

Jump to solution
2,036 Views
bobgardner
Contributor I

Part of CW? Part of the EVB?

Labels (1)
0 Kudos
Reply
1 Solution
1,878 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Bob

The head file <hidef.h> locates at the default system path:

C:\Program Files (x86)\Freescale\CWS12v5.1\lib\hc12c\include

Please open the Target Settings by ‘ALT’+’F7’, can check whether the system path is configured correctly in your project.

system path.png

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

  ---------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,879 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Bob

The head file <hidef.h> locates at the default system path:

C:\Program Files (x86)\Freescale\CWS12v5.1\lib\hc12c\include

Please open the Target Settings by ‘ALT’+’F7’, can check whether the system path is configured correctly in your project.

system path.png

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

  ---------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply