Can't open my project anymore

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't open my project anymore

ソリューションへジャンプ
2,443件の閲覧回数
MAPC
Senior Contributor I

Hello, dears

 

My project was running ok. Suddenly, when I open Code Warrior 10.5, it pops us the following message:

 

11914_11914.jpgproj_open_error.jpg

 

And since then, I just can't open the project anymore. When I close a message, another one comes up, and this never ends. It is curious that this happens with only one project in my workspace. The other project can be opened without problems. I couldn't identify the reason for that. Probably, one or more files might be corrupted, I don't know.

 

Did anybody face such a problem?

 

 

Regards,

 

Marco Coelho

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,128件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It might be something with the parallel build settings?

Can you try the fix mentioned in CW ProjectsView Project Loading Verification Internal Error

?

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,128件の閲覧回数
MAPC
Senior Contributor I

Hi, Erich

I just tried it and worked perfectly.

The doesn't ocurr only with QG8. In my project, I used MC9S08PA8. It seems like a kind of bug in Code Warrior v. 10.5?

I hope that was solved in Code Warrior v. 10.6.

Thank you very much!

Marco Coelho

0 件の賞賛
返信
2,129件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It might be something with the parallel build settings?

Can you try the fix mentioned in CW ProjectsView Project Loading Verification Internal Error

?

0 件の賞賛
返信
2,128件の閲覧回数
MAPC
Senior Contributor I

Hi, Erich

I just tried it and worked perfectly.

The doesn't ocurr only with QG8. In my project, I used MC9S08PA8. It seems like a kind of bug in Code Warrior v. 10.5?

I hope that was solved in Code Warrior v. 10.6.

Thank you very much and congratulations for your valuable job on mcuoneclipse.com!

Marco Coelho

0 件の賞賛
返信