Can't find the SDA connection on Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't find the SDA connection on Flash

1,873件の閲覧回数
shiroe0329
Contributor I

Hello everyone

In my case.

I can find my PEMicro OpenSDA Debug Drive in Jungo also can debug.

But when I want to flash the target to my board(KEAZN64).

It can't find the connection and when I create a new connection.

It will get a storage error and can't get the target program to my board.

Can anyone help me to slove this problem?

Thanks a lot!!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,805件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

From your screenshot , it seems you use the Flash File to Target function,

there is a introduce about it  of the attachment :

3.12 Flash File to Target

If you still have question , please show the steps one by one about how do you

configure it,  then i can reproduce it on my side .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,805件の閲覧回数
shiroe0329
Contributor I

Thanks Alice

I found the problem finally

Cauz I use Debug then forget to stop it

That's why I can't use Flash the target file

Thanks for your reply again!

0 件の賞賛
返信