Can't connect to HCS08 device in Freemaster using PE Micro Multilink FX but non FX Multilinks work fine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't connect to HCS08 device in Freemaster using PE Micro Multilink FX but non FX Multilinks work fine

ソリューションへジャンプ
2,742件の閲覧回数
jer
Contributor II

I bought a PE Micro Multilink FX because its supposed to be a bit more robust and we've fried a couple standard ones in our test environment.  I can successfully program and debug parts using the Multilink FX in Codewarrior but can't seem to connect in Freemaster.  The standard Multilink works fine in Freemaster.  

It looks like during the connection wizard when HCS08 is selected for driver it can't find a device using the FX.  If I select any of the other drivers it can find the device just fine.  

I've uninstalled and reinstalled the drivers, both PE and Freemaster, it did not change anything.

Using Freemaster version 2.0.7.0 and Windows 10

タグ(2)
0 件の賞賛
返信
1 解決策
2,578件の閲覧回数
jer
Contributor II

I contacted PE Micro and they sent me a new DLL to replace one in the Freemaster program.  It works fine now.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,579件の閲覧回数
jer
Contributor II

I contacted PE Micro and they sent me a new DLL to replace one in the Freemaster program.  It works fine now.

0 件の賞賛
返信