Can't build a fuction that should return a structure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't build a fuction that should return a structure

1,238 次查看
juanignaciotroi
Contributor III

Hello. I am developing using de FRDMKE02 and using the CW Sevelopment Studio. In my project, I have defined the following structure for dealing with time:

 

typedef struct TimeStruct {

  unsigned char SECONDS;

  unsigned char MINUTES;

  unsigned char HOURS;

  unsigned char DAY_OF_THE_WEEK;

  unsigned char DATE;

  unsigned char MONTH;

  unsigned char YEAR;

};

 

I have done a fuction in which I want to add a determined quantity of time (days, hours and minutes; defined by char add_dd, char add_hh and char add_mm respectively)  to the entrant TimeStruct and then it should return the resulting TimeStruct. The problem is that I can't even build this fuction.

The error log says that: "return type is an incomplete type".

 

I hope someone can help me. Regards, Juan Ignacio Troisi

 

 

The intended function is:

 

struct TimeStuct sumar_horas_y_minutos(struct TimeStruct TIEMPO_SUMADO,char add_dd,char add_hh,char add_mm){

 

  TIEMPO_SUMADO.MINUTES = TIEMPO_SUMADO.MINUTES + add_mm;

 

  if(TIEMPO_SUMADO.MINUTES > 59){

 

  TIEMPO_SUMADO.HOURS ++;

  TIEMPO_SUMADO.MINUTES = TIEMPO_SUMADO.MINUTES - 60;

 

  }

 

  TIEMPO_SUMADO.HOURS = TIEMPO_SUMADO.HOURS + add_hh;

 

  if(TIEMPO_SUMADO.HOURS >= 24){

 

  TIEMPO_SUMADO.DATE ++;

  TIEMPO_SUMADO.HOURS = TIEMPO_SUMADO.HOURS - 24;

 

  }

 

  TIEMPO_SUMADO.DATE = TIEMPO_SUMADO.DATE + add_dd;

 

 

 

  switch_month(TIEMPO_SUMADO);

 

  if(TIEMPO_SUMADO.MONTH > 12){

 

  TIEMPO_SUMADO.YEAR ++;

  TIEMPO_SUMADO.MONTH = TIEMPO_SUMADO.MONTH -12;

 

  }

 

 

 

 

 

  return TIEMPO_SUMADO;

 

}

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,100 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Juan Ignacio Troisi:

There is a typo in your code:

pastedImage_0.png

That should be TimeStruct. Also for the typedef you should declare an identifier name.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,100 次查看
juanignaciotroi
Contributor III

Thank you but, unfortunately, I can't build build the project yet.

When I don't call the function, it builds. However, when I want to use it (it calling doing: 'sumar_horas_y_minutos(TIEMPO_SUMADO,add_dd,add_hh,add_mm);', the following error turns up:

"conflicting types for sumar_horas_y_minutos".

the code is:

struct TimeStruct sumar_horas_y_minutos(struct TimeStruct TIEMPO_SUMADO,char add_dd,char add_hh,char add_mm){

  TIEMPO_SUMADO.MINUTES = TIEMPO_SUMADO.MINUTES + add_mm;

  if(TIEMPO_SUMADO.MINUTES > 59){

  TIEMPO_SUMADO.HOURS ++;

  TIEMPO_SUMADO.MINUTES = TIEMPO_SUMADO.MINUTES - 60;

  }

  TIEMPO_SUMADO.HOURS = TIEMPO_SUMADO.HOURS + add_hh;

  if(TIEMPO_SUMADO.HOURS >= 24){

  TIEMPO_SUMADO.DATE ++;

  TIEMPO_SUMADO.HOURS = TIEMPO_SUMADO.HOURS - 24;

  }

  TIEMPO_SUMADO.DATE = TIEMPO_SUMADO.DATE + add_dd;

  switch_month(TIEMPO_SUMADO);

  if(TIEMPO_SUMADO.MONTH > 12){

  TIEMPO_SUMADO.YEAR ++;

  TIEMPO_SUMADO.MONTH = TIEMPO_SUMADO.MONTH -12;

  }

  return TIEMPO_SUMADO;

}

Thanks

0 项奖励
回复