CW11.1 license error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW11.1 license error

跳至解决方案
843 次查看
leolv
Contributor II

leolv_1-1735634072618.png

 
Installed Products:
 - CodeWarrior for MCU
Version: 11.1
Build Id:181224

 

#above is version and license information

#but when i open the IDE it always report errors below

leolv_2-1735634218409.png

how to fix this issue

In addition i am not sure where i should place my licesne.dat in client side.

 

 

0 项奖励
回复
1 解答
815 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @leolv ,

Thanks for your post. From your picture, it shows that your license.dat is in the right place and has been activated successfully. There's no problem. Regarding the log "CDE: no license found, using Community Edition License", it is not an error log but a normal one, and the appearance of this message will not affect the normal use of CodeWarrior. CDE means the Component Development Environment. You can refer to the link below for more details.

Solved: What tool do I kneed for Component Development? - NXP Community

In short, this log is not an error and won't affect your use. 

Hope it can help you. 

BRs,

Celeste

---------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------

 

在原帖中查看解决方案

1 回复
816 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @leolv ,

Thanks for your post. From your picture, it shows that your license.dat is in the right place and has been activated successfully. There's no problem. Regarding the log "CDE: no license found, using Community Edition License", it is not an error log but a normal one, and the appearance of this message will not affect the normal use of CodeWarrior. CDE means the Component Development Environment. You can refer to the link below for more details.

Solved: What tool do I kneed for Component Development? - NXP Community

In short, this log is not an error and won't affect your use. 

Hope it can help you. 

BRs,

Celeste

---------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------