CW10.2的license报错问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.2的license报错问题

2,336 Views
yangweijason
Contributor I

您好,我测试对时,调整系统时间后,发现CodeWorrior10.2的license报错了。报错:功能 ProfessionalEditionMCU 10.2,状态: KeyProfessionalEditionMCU, LM_BADSYSDATE出现未知错误。我反复重装软件无法解决,希望帮我解决问题,谢谢。

0 Kudos
Reply
11 Replies

1,837 Views
yangweijason
Contributor I

license应该是没问题,同事用过的。i详细情况如下:

细节信息:产品"MCU Wizard and Tools Plugins" 版本"10.2.0.FSL_b03041"
状态:"KeyProfessionalEditionMCU 10.2, LM_BADSYSDATE出现未知错误。 "
License模式:"class com.freescale.core.ide.license.flexlm.FlexlmActivate11"
联系电子邮件:licensing@freescale.com
注册URL:http://www.freescale.com/cwregister
购买URL: http://www.freescale.com/cwmcu10
FlexLM评估期还有:15 天
GTL服务器:gtlsrvr.metrowerks.com
GTL端口:80 (8,080)
需要Host ID: true
License文件路径:D:\CWMCU\CW MCU v10.2\MCU\license.dat
flexlmFileLocator: null
flexlmFile: ${MCU_TOOLS_HOME}/license.dat
License文件URL: file:/D:/CWMCU/CW MCU v10.2/eclipse/../MCU/license.dat
错误字段: KeyProfessionalEditionMCU 10.2, LM_BADSYSDATE出现未知错误。
功能Key:
功能 ProfessionalEditionMCU 10.2,状态: KeyProfessionalEditionMCU, LM_BADSYSDATE出现未知错误。
替代Key:
(没有key)
LM_PATH=null
许可文件内容({0}):
~INCREMENT ProfessionalEditionMCU metrowks 10.2 23-nov-2018 uncounted \
BE8C421D967A VENDOR_STRING="Professional Edition MCU 10.2 " \
HOSTID=ANY TS_OK

0 Kudos
Reply

1,837 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Do you use 30-day evaluation license or purchased permanent license?

Jennie Zhang

0 Kudos
Reply

1,837 Views
yangweijason
Contributor I

yes,I have use 30-day evaluation license,how can i do?

0 Kudos
Reply

1,837 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

We can't change computer system time when using evaluation license, because evaluation license is bounded with date/time.

When will your license expire? Normally one user can apply evaluation twice totally.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,837 Views
yangweijason
Contributor I

INCREMENT ProfessionalEditionMCU metrowks 10.2 23-nov-2018 uncounted 。

2018年11月23号过期。但是现在软件用不了,软件的license之前一直是国内芯片供应商提供的,后来闲麻烦就用了试用版本license,我是测试PC机是否对时成功才修改时间,搞出问题了,希望您给一个解决方案,谢谢了。拜托。

0 Kudos
Reply

1,837 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

what I got from you: your evaluation license expire time 23-nov-2018. If you use this evaluation license without changing system time, it works fine. If you change system time, this evaluation license produce error.

Correct?

0 Kudos
Reply

1,837 Views
yangweijason
Contributor I

你的理解是对的。改过系统时间后,就不能正常工作,现在系统不管时间是否是修改过的,软件都不能正常工作。现在我是一直无法使用软件。

0 Kudos
Reply

1,837 Views
BlackNight
NXP Employee
NXP Employee

FYI, LM_BADSYSDATE means that the licensing system has detected a 'clock setting back' scenario, meaning a tampering of the system to extend the evaluation period. This means FLEXlm won't allow you to run any time limited licenses any more.

0 Kudos
Reply

1,837 Views
yangweijason
Contributor I

您好,再请教一个问题。如下:

问题描述:K10的三个SPI采样八路AD芯片,带Jlink仿真的时候采样数据正常,去掉Jlink单跑采样数据大约是之前的一般,像丢失高位的样子
0 Kudos
Reply

1,837 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

This is a new question about Kinestis. Please post new question to

https://community.nxp.com/community/kinetis 

0 Kudos
Reply

1,837 Views
yangweijason
Contributor I

求大神帮忙解决

0 Kudos
Reply