CW 5.2 for HCS12(x)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW 5.2 for HCS12(x)

1,619 次查看
tnriley
Contributor III

I have been able to get a node locked licensed version of CW 5.1 to run correctly on a non-networked win7-64 machine. I have attempted to download the version 5.2 update and install on the same machine. However, the 5.2 version does not have all of the processor options available that are included in 5.1 version. In fact it is a greatly limited listing of those available in 5.1. Is there another download somewhere that I am missing?

 

I am using this page for downloads

CodeWarrior for HC12 Professional Edition WIN

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7153847 

 

Also, is there a method to perform an update rather than a new install from 5.1 to 5.2? This is a non-networked machine.

标签 (1)
0 项奖励
回复
1 回复

1,507 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim,

CW 5.2 can only support limited device.  this is a market decision.

 

This release includes support for the following derivatives:
    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
    - MC9S12G128, MC9S12G96
    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
    - MC9S12GN16, MC9S12GN32
    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
    - MC9S12XEP100, MC9S12XEP768
    - MC9S12XEQ384, MC9S12XEQ512
    - MC9S12XET256
    - MC9S12XS128, MC9S12XS256, MC9S12XS64
    - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

 

I wrote an article about how to install missing device to CW v5.2

https://community.freescale.com/docs/DOC-330657


My suggestion for you is to use CW5.1 instead. attached is how to download CW5.1. Hope this helps.

 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------