Hi all,
creating project with Processor Expert, as last step of the build the burner is invoked to create the .s19 file.
I created a new project with no Processor Expert support and I cannot find in the Properties // C/C++ Settings // Tool Settings
how to enable the creation of the .s19 file.
Could you please explain me how to do this?
Thanks for your time
Hi,
I created a new project and copied my files into it, then updated the project settings. I succeeded in creating a hex file. But I didn't succeed by downloading it with tftp.
I will concentrate back to CW10.5 and MQX4.0.1. All this is not reliable.. At this point I'm not sure I can finish my project with freescale. I will open other topics for my current problems and try to solve them.
BR
stephan
I just tried to create a new basic project linked to my local MQX with my specific BSP as I use it normally. It's ok, I can get the Hex file.. So I have no clue why for my project it doesn't work.
And I don't know what to look..
Hi Stephan,
I think It could be interesting if we could reproduce the problem on our side too.
Is it possible to have the project ?
Now if you don't want to share it on community we can continue through Service Request system.
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
yes, strange.
It looks like a problem with the parallel build settings. Can you try to disable it:
Erich
i just tried that 5 minutes ago. :-)
No changes..
If I check the "Problems" tabs under warnings I have those 2 line for the makefile that I get only in release:
| Description | Resource | Path | Location | Type | 
| make: ignoring old recipe for target `OSV8_Camera.elf' | makefile | /OSV8_Camera/twrk60f120m_Int_Flash_Release | line 77 | C/C++ Problem | 
| make: overriding recipe for target `OSV8_Camera.elf' | makefile | /OSV8_Camera/twrk60f120m_Int_Flash_Release | line 113 | C/C++ Problem | 
Stephan
Could you post your complete console log (copy-paste the text)?
I believe that the link phase failed, but cannot tell from your screenshot.
Maybe you have custom options set per files/folder?
This is a problem with objcopy (see Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse).
Erich
Here it is:
I will check your link in parallel.
**** Build of configuration twrk60f120m_Int_Flash_Release for project OSV8_Camera ****
"C:\\Freescale\\CW MCU v10.6\\gnu\\bin\\mingw32-make" -j16 pre-build main-build
SubWCRev.exe E:\Mes_Projets\OSV8\CW10_6_OSV8\OSV8_Camera E:\Mes_Projets\OSV8\CW10_6_OSV8\OSV8_Camera\Sources\SvnInfo.tmpl E:\Mes_Projets\OSV8\CW10_6_OSV8\OSV8_Camera\Sources\SvnInfo.h
SubWCRev : E155007: 'E:\Mes_Projets\OSV8\CW10_6_OSV8\OSV8_Camera' is not a working copy
' '
'Building file: ../Sources/main.c'
'Building file: ../Sources/Utils/stbp/StTime.c'
'Building file: ../Sources/Utils/stbp/stbp.c'
'Building file: ../Sources/Utils/RTCS_Lib/CGI.c'
'Building file: ../Sources/Utils/RTCS_Lib/Driver_DP83640.c'
'Building file: ../Sources/Utils/RTCS_Lib/PTPv2.c'
'Building file: ../Sources/Utils/RTCS_Lib/RTCS_Init.c'
'Building file: ../Sources/Utils/RTCS_Lib/RTCS_Socket.c'
'Building file: ../Sources/Drivers/AdcDriver.c'
'Building file: ../Sources/Drivers/ExtEeprom.c'
'Building file: ../Sources/Drivers/LensH16Driver.c'
'Building file: ../Sources/Drivers/LensXA20Driver.c'
'Building file: ../Sources/Control/StbpCamera.c'
'Building file: ../Sources/Application/CommunicationManager.c'
'Building file: ../Sources/Application/timer.c'
'Executing target #1 ../Sources/main.c'
'Executing target #2 ../Sources/Utils/stbp/StTime.c'
'Executing target #3 ../Sources/Utils/stbp/stbp.c'
'Executing target #4 ../Sources/Utils/RTCS_Lib/CGI.c'
'Executing target #5 ../Sources/Utils/RTCS_Lib/Driver_DP83640.c'
'Executing target #6 ../Sources/Utils/RTCS_Lib/PTPv2.c'
'Executing target #7 ../Sources/Utils/RTCS_Lib/RTCS_Init.c'
'Executing target #8 ../Sources/Utils/RTCS_Lib/RTCS_Socket.c'
'Executing target #9 ../Sources/Drivers/AdcDriver.c'
'Executing target #10 ../Sources/Drivers/ExtEeprom.c'
'Executing target #11 ../Sources/Drivers/LensH16Driver.c'
'Executing target #12 ../Sources/Drivers/LensXA20Driver.c'
'Executing target #13 ../Sources/Control/StbpCamera.c'
'Executing target #14 ../Sources/Application/CommunicationManager.c'
'Executing target #15 ../Sources/Application/timer.c'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
'Invoking: ARM Ltd Windows GCC C Compiler'
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/main.c" @"Sources/main.args" -Wa,-adhlns="Sources/main.o.lst" -MMD -MP -MF"Sources/main.d" -o"Sources/main.o"
'Invoking: ARM Ltd Windows GCC C Compiler'
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Utils/stbp/StTime.c" @"Sources/Utils/stbp/StTime.args" -Wa,-adhlns="Sources/Utils/stbp/StTime.o.lst" -MMD -MP -MF"Sources/Utils/stbp/StTime.d" -o"Sources/Utils/stbp/StTime.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Utils/stbp/stbp.c" @"Sources/Utils/stbp/stbp.args" -Wa,-adhlns="Sources/Utils/stbp/stbp.o.lst" -MMD -MP -MF"Sources/Utils/stbp/stbp.d" -o"Sources/Utils/stbp/stbp.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Utils/RTCS_Lib/CGI.c" @"Sources/Utils/RTCS_Lib/CGI.args" -Wa,-adhlns="Sources/Utils/RTCS_Lib/CGI.o.lst" -MMD -MP -MF"Sources/Utils/RTCS_Lib/CGI.d" -o"Sources/Utils/RTCS_Lib/CGI.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Utils/RTCS_Lib/Driver_DP83640.c" @"Sources/Utils/RTCS_Lib/Driver_DP83640.args" -Wa,-adhlns="Sources/Utils/RTCS_Lib/Driver_DP83640.o.lst" -MMD -MP -MF"Sources/Utils/RTCS_Lib/Driver_DP83640.d" -o"Sources/Utils/RTCS_Lib/Driver_DP83640.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Utils/RTCS_Lib/PTPv2.c" @"Sources/Utils/RTCS_Lib/PTPv2.args" -Wa,-adhlns="Sources/Utils/RTCS_Lib/PTPv2.o.lst" -MMD -MP -MF"Sources/Utils/RTCS_Lib/PTPv2.d" -o"Sources/Utils/RTCS_Lib/PTPv2.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Utils/RTCS_Lib/RTCS_Init.c" @"Sources/Utils/RTCS_Lib/RTCS_Init.args" -Wa,-adhlns="Sources/Utils/RTCS_Lib/RTCS_Init.o.lst" -MMD -MP -MF"Sources/Utils/RTCS_Lib/RTCS_Init.d" -o"Sources/Utils/RTCS_Lib/RTCS_Init.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Utils/RTCS_Lib/RTCS_Socket.c" @"Sources/Utils/RTCS_Lib/RTCS_Socket.args" -Wa,-adhlns="Sources/Utils/RTCS_Lib/RTCS_Socket.o.lst" -MMD -MP -MF"Sources/Utils/RTCS_Lib/RTCS_Socket.d" -o"Sources/Utils/RTCS_Lib/RTCS_Socket.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Drivers/AdcDriver.c" @"Sources/Drivers/AdcDriver.args" -Wa,-adhlns="Sources/Drivers/AdcDriver.o.lst" -MMD -MP -MF"Sources/Drivers/AdcDriver.d" -o"Sources/Drivers/AdcDriver.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Drivers/ExtEeprom.c" @"Sources/Drivers/ExtEeprom.args" -Wa,-adhlns="Sources/Drivers/ExtEeprom.o.lst" -MMD -MP -MF"Sources/Drivers/ExtEeprom.d" -o"Sources/Drivers/ExtEeprom.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Drivers/LensH16Driver.c" @"Sources/Drivers/LensH16Driver.args" -Wa,-adhlns="Sources/Drivers/LensH16Driver.o.lst" -MMD -MP -MF"Sources/Drivers/LensH16Driver.d" -o"Sources/Drivers/LensH16Driver.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Drivers/LensXA20Driver.c" @"Sources/Drivers/LensXA20Driver.args" -Wa,-adhlns="Sources/Drivers/LensXA20Driver.o.lst" -MMD -MP -MF"Sources/Drivers/LensXA20Driver.d" -o"Sources/Drivers/LensXA20Driver.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Control/StbpCamera.c" @"Sources/Control/StbpCamera.args" -Wa,-adhlns="Sources/Control/StbpCamera.o.lst" -MMD -MP -MF"Sources/Control/StbpCamera.d" -o"Sources/Control/StbpCamera.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Application/CommunicationManager.c" @"Sources/Application/CommunicationManager.args" -Wa,-adhlns="Sources/Application/CommunicationManager.o.lst" -MMD -MP -MF"Sources/Application/CommunicationManager.d" -o"Sources/Application/CommunicationManager.o"
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-gcc" "../Sources/Application/timer.c" @"Sources/Application/timer.args" -Wa,-adhlns="Sources/Application/timer.o.lst" -MMD -MP -MF"Sources/Application/timer.d" -o"Sources/Application/timer.o"
'Finished building: ../Sources/Drivers/LensXA20Driver.c'
' '
'Finished building: ../Sources/Application/CommunicationManager.c'
'Finished building: ../Sources/Utils/RTCS_Lib/Driver_DP83640.c'
' '
' '
'Finished building: ../Sources/Utils/stbp/StTime.c'
' '
'Finished building: ../Sources/Utils/RTCS_Lib/RTCS_Init.c'
'Finished building: ../Sources/Drivers/ExtEeprom.c'
' '
' '
'Finished building: ../Sources/Drivers/AdcDriver.c'
' '
'Finished building: ../Sources/Utils/RTCS_Lib/PTPv2.c'
' '
'Finished building: ../Sources/Drivers/LensH16Driver.c'
'Finished building: ../Sources/Utils/stbp/stbp.c'
' '
' '
'Finished building: ../Sources/Control/StbpCamera.c'
'Finished building: ../Sources/Application/timer.c'
' '
' '
'Finished building: ../Sources/Utils/RTCS_Lib/CGI.c'
' '
'Finished building: ../Sources/main.c'
' '
'Finished building: ../Sources/Utils/RTCS_Lib/RTCS_Socket.c'
' '
'Executing target #17 OSV8_Camera.hex'
'Invoking: ARM Ltd Windows GNU Create Flash Image'
“C:/Freescale/CW MCU v10.6\eclipse\../Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-objcopy” -O srec --srec-len=252 OSV8_Camera.elf "OSV8_Camera.hex"
makefile:113: warning: overriding recipe for target `OSV8_Camera.elf'
makefile:77: warning: ignoring old recipe for target `OSV8_Camera.elf'
mingw32-make: [pre-build] Error 10 (ignored)
In file included from E:/Mes_Projets/OSV8/CW10_6_OSV8/OSV8_Camera/Sources/Typedef.h:16:0,
from ../Sources/Utils/stbp/stbp.h:25,
from ../Sources/Utils/stbp/stbp.c:21:
E:/Mes_Projets/OSV8/CW10_6_OSV8/OSV8_Camera/Sources/SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Utils/stbp/StTime.c:98:97: warning: 'uPrecisionFactor' may be used uninitialized in this function [-Wmaybe-uninitialized]
../Sources/main.c:98:11: warning: unused variable 'dummy' [-Wunused-variable]
../Sources/main.c:373:4: warning: implicit declaration of function '_event_create_component' [-Wimplicit-function-declaration]
../Sources/main.c:381:4: warning: implicit declaration of function '_event_create' [-Wimplicit-function-declaration]
../Sources/main.c:407:2: warning: dereferencing 'void *' pointer [enabled by default]
../Sources/Utils/stbp/StTime.c:180:39: warning: 'uPrecisionFactor' may be used uninitialized in this function [-Wmaybe-uninitialized]
E:/Mes_Projets/OSV8/CW10_6_OSV8/OSV8_Camera/Sources/SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Utils/stbp/StTime.c:293:41: warning: 'iTicks24h' may be used uninitialized in this function [-Wmaybe-uninitialized]
E:/Mes_Projets/OSV8/CW10_6_OSV8/OSV8_Camera/Sources/SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Utils/RTCS_Lib/PTPv2.c:806:1: warning: missing braces around initializer [-Wmissing-braces]
../Sources/Utils/RTCS_Lib/PTPv2.c:831:11: warning: variable 'varRead' set but not used [-Wunused-but-set-variable]
../Sources/Utils/RTCS_Lib/PTPv2.c:856:13: warning: unused variable 'inBuff_ptr' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/PTPv2.c:855:12: warning: unused variable 'outTrameTmp' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/PTPv2.c:971:11: warning: variable 'varTmp' set but not used [-Wunused-but-set-variable]
../Sources/Utils/RTCS_Lib/PTPv2.c:1045:10: warning: unused variable 'correctionPhy' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/PTPv2.c:1203:19: warning: unused variable 'timestampOftrame' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/PTPv2.c:1319:26: warning: variable 'msec' set but not used [-Wunused-but-set-variable]
../Sources/Utils/RTCS_Lib/PTPv2.c:1450:10: warning: unused variable 'phyClock' [-Wunused-variable]
../Sources/Drivers/..\SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Drivers/LensXA20Driver.c:41:9: warning: unused variable 'dummy' [-Wunused-variable]
../Sources/Drivers/..\SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Drivers/ExtEeprom.c:184:30: warning: unused variable 'i' [-Wunused-variable]
../Sources/Drivers/ExtEeprom.c:199:30: warning: unused variable 'i' [-Wunused-variable]
E:/Mes_Projets/OSV8/CW10_6_OSV8/OSV8_Camera/Sources/SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Application/CommunicationManager.c:449:7: warning: implicit declaration of function 'abs' [-Wimplicit-function-declaration]
../Sources/Application/CommunicationManager.c:730:2: warning: value computed is not used [-Wunused-value]
../Sources/Application/CommunicationManager.c:62:14: warning: 'alreadyInPrintf' defined but not used [-Wunused-variable]
E:/Mes_Projets/OSV8/CW10_6_OSV8/OSV8_Camera/Sources/SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Utils/RTCS_Lib/RTCS_Socket.c:32:6: warning: unused variable 'option' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/RTCS_Socket.c:100:10: warning: unused variable 'length' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/RTCS_Socket.c:99:11: warning: unused variable 'error' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/RTCS_Socket.c:98:11: warning: unused variable 'index' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/RTCS_Socket.c:375:11: warning: unused variable 'error' [-Wunused-variable]
../Sources/Utils/RTCS_Lib/RTCS_Socket.c:396:11: warning: unused variable 'handle' [-Wunused-variable]
../Sources/Application/CommunicationManager.c:466:14: warning: 'refInc' may be used uninitialized in this function [-Wmaybe-uninitialized]
../Sources/Application/CommunicationManager.c:543:14: warning: 'refAccZ' may be used uninitialized in this function [-Wmaybe-uninitialized]
../Sources/Application/CommunicationManager.c:535:14: warning: 'refAccY' may be used uninitialized in this function [-Wmaybe-uninitialized]
../Sources/Application/CommunicationManager.c:527:14: warning: 'refAccX' may be used uninitialized in this function [-Wmaybe-uninitialized]
../Sources/Application/CommunicationManager.c:459:14: warning: 'ref12V' may be used uninitialized in this function [-Wmaybe-uninitialized]
../Sources/Application/CommunicationManager.c:436:10: warning: 'ref54V' may be used uninitialized in this function [-Wmaybe-uninitialized]
E:/Mes_Projets/OSV8/CW10_6_OSV8/OSV8_Camera/Sources/SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Utils/RTCS_Lib/Driver_DP83640.c:43:2: warning: implicit declaration of function 'MACNET_write_mii' [-Wimplicit-function-declaration]
../Sources/Utils/RTCS_Lib/Driver_DP83640.c:65:2: warning: implicit declaration of function 'MACNET_read_mii' [-Wimplicit-function-declaration]
../Sources/Utils/RTCS_Lib/Driver_DP83640.c:430:5: warning: implicit declaration of function 'abs' [-Wimplicit-function-declaration]
../Sources/Utils/RTCS_Lib/Driver_DP83640.c:383:10: warning: unused variable 'nsecTemp' [-Wunused-variable]
../Sources/Control/StbpCamera.c:84:2: warning: implicit declaration of function 'CommunicationManager_SendToPC' [-Wimplicit-function-declaration]
../Sources/Control/StbpCamera.c:98:2: warning: implicit declaration of function 'GetConvertedInclinometer' [-Wimplicit-function-declaration]
../Sources/Control/StbpCamera.c:111:2: warning: implicit declaration of function 'GetConvertedTemparture' [-Wimplicit-function-declaration]
../Sources/Control/StbpCamera.c:340:2: warning: implicit declaration of function 'CommunicationManager_SendTime' [-Wimplicit-function-declaration]
../Sources/Control/StbpCamera.c:1329:7: warning: dereferencing 'void *' pointer [enabled by default]
../Sources/Control/StbpCamera.c:1355:7: warning: dereferencing 'void *' pointer [enabled by default]
../Sources/Application/..\SystemDefinitions.h:502:2: warning: parameter names (without types) in function declaration [enabled by default]
../Sources/Application/timer.c:78:4: warning: implicit declaration of function 'abs' [-Wimplicit-function-declaration]
../Sources/Application/timer.c:260:2: warning: implicit declaration of function '_event_open' [-Wimplicit-function-declaration]
mingw32-make: *** [OSV8_Camera.hex] Error 1
Hi,
I have a project based on K60F120M that was "working" with CW10.5 and MQX4.0. As I have some problem with TCP IP /UDP connections I'm trying with CW10.6 and MQX4.1.1.
For that I created I new project in my new environment and after that I updated the project files with my files. (to have all new from CW10.6)
I finally succeded in building libraries and project and run it in debug mode. Now I'm trying the release version.
I found here that it needs to add in the project properties the "Create Flash Image" to get the srecord file to download with my bootloader.
My problem is that I always get an error and once the option "Create Flash Image" is activated I cannot get neither the ELF or HEX software file.
I am lost. Nothing in the links I found explain that...
Thanks
BR
stephan
Hi Stephan,
With the MCU v10.6 + MQX V4.1.1, I've create a project via the wizard for MQX Hello example.
The board used is K60F120M too.
Before to build the project I've build the MQX libraries.
Attached you will find a video showing how I've selected the Create Flash Image under Addtional Tools.
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks for the video, it is exactly what I did. It seems that the ELF file disappear and then it's not find to create the S19.
As I still have to get working with some points I went back on CW10.5 and MQX4.0.1. If you have some other comments or suggestions it's welcome, I will try ASAP again.
Thanks
BR
stephan
Stephan,
The file created is not named .s19.
Under MCU V10.x the file is named with .hex as showed in the video.
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
Yes I know. :-) I was thinking about that after the renaming. (option in commands to do it automatically)
But I tried with renaming, just create the HEX-file as you mentionned and it crashes. I will try again today.
Thanks
BR
Stephan
See
http://mcuoneclipse.com/2012/09/13/s-record-generation-with-gcc-for-armkinetis/
I hope this helps,
Erich
Hi Eric,
thanks for your reply.
Unfortunately I forgot to point out that I am using a S08PT and the C/C++ Settings tab is
significantly different from the Kinetis version (i.e. I cannot find any Additional Tools tab.
I solved my problem adding the burning step in the post-building steps
but I'm still searching a more "out-of-the-box" solution. It must be there, somewhere. :smileyhappy:
Thanks anyway for all your suggestions.
FP
Hello Francesco:
There is indeed an option to create S19 file. This is in Project -> Properties -> C/C++ Build -> Settings -> Tool Settings -> S08 Linker -> Output:
However, I have seen that for S08 projects, the burner is invoked by default from the makefile, so the S19 file should be generated without that option enabled. If you are not getting the S19 file generated, it could be caused by Per-File settings, explained by Erich himself at the next tutorial:
Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse
With custom file settings the makefile is not generated properly.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------