Burn a new RCW to T4240RDB Rev2 board with CW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Burn a new RCW to T4240RDB Rev2 board with CW

1,065 Views
sedat_sedat
Contributor I

Hello,

I am trying to write RCW to NOR Flash of a T4240RDB Rev2 board with a broken RCW on EEPROM. 

I am using codewarrior "CodeWarrior_PA_10.5.1"

 

I created an new Bareboard project with target T4240RDB Rev2.

I am using the SRAM download project with T4240RDB_RCW_1666_733_1867-rev2.0.txt as jtag initialization file.

T4240RDB_init_sram.tcl Target initialization file. and T4240RDB.mem memory initialization

 

Using CodeWarrior TAP over ethernet.

The switch settings of the T4240RDB board is done as written in T4240RDB_eabi_README.txt 

SW1: 1100 SW2 :1111 SW3:1111 SW4:1111

And the jumper1 JP1 is at JTAG mode.

When I start the debug sessin I got the message: 

"CCSProtocolPlugin: Failed to correctly configure the JTAG chain."

Does anybody have any idea about this case, since T4240RDB is the reference board of NXP not my custom design, in my opinion  I think it must be easy to connect and burn a new RCW .

Does anybody have any idea, any help will be appreciated.

 

 

0 Kudos
Reply
1 Reply

817 Views
sedat_sedat
Contributor I

Instead of using jtag for RCW  I solved the problem by writing the RCW to SD card and boot from SD. 

Then I wrote the RCW to eeprom from uboot.

0 Kudos
Reply