Build project with a makefile, can rebuild but can't build.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build project with a makefile, can rebuild but can't build.

Jump to solution
1,795 Views
pamis
Contributor II

Hi,

    I need build my application for S12VR48 with a makefile project. Hence, i extended the sample MakeFileSample_HC12 from "CWS12v5.2/(CodeWarrior_Examples)" direction.

    Now, i extended the sample complete. I can use rebuild command successful, but can't use build command.

 

It report error as following:

Reading make file 'F:\Workspace\trunk\Skylight\Project\makefile.mak' F:\Workspace\trunk\Skylight\Project\makefile.mak: ERROR M5022: Don't know how to make "etimer.s" F:\Workspace\trunk\Skylight\Project\makefile.mak: ERROR M5022: Don't know how to make "etimer.o" F:\Workspace\trunk\Skylight\Project\makefile.mak: ERROR M5022: Don't know how to make "Project.abs" F:\Workspace\trunk\Skylight\Project\makefile.mak: ERROR M5022: Don't know how to make "all" F:\Workspace\trunk\Skylight\Project\makefile.mak: ERROR M5022: Don't know how to make "all"

Here is my makefile: 

 

############################## Auto-make file: default.mak############################## Following variables should be updated to reflect you current project settings.# PROJECT:                                      Project name. Name of the final absolute/S19/library file,#                       without path informationPROJECT=Project # SOURCE_FILES:                                 All C/C++/ASM files (without path)SOURCE_FILES=datapage.c Start12.c main.c mc9s12vr48.c clock.c etimer.c process.c stimer.c timer.c Hal.c Hil.c Anti-pinch.c Diagnose.c SafeRank.c MotorClass.c Debug.c Motor.c Operation.c RealtmSt.c Skylight.c # ADD_OBJECTS:                                  Additional object/library files to link withADD_OBJECTS=ansisf.lib # INSTALLPATH:          Path where tools are installed (root installation#                       directory). If called from build.bat, INSTALLPATH#                       is through -D option.#                       Remove comment below and adjust path if INSTALLPATH is not#                       set on make invocation line#INSTALLPATH=C:\Freescale\CodeWarrior_HC12# LINKFILE:             Linker parameter file to be usedLINKFILE=.\prm\project.prm# MAKEFILE:             Name of this make fileMAKEFILE=makefile.mak # define here if you want to build a absolute file (abs) or a library (lib)BUILD_TARGET_EXT=abs#BUILD_TARGET_EXT=lib#INCLUDEPATH:           Paths where application or system include files can be#                       found.INCLUDEPATH="$(INSTALLPATH)\lib\hc12c\include"#".\Sources\user\arch";#".\Sources";#".\Sources\user\bsw";".\Sources\user\module";".\Sources\user\oop";".\Sources\user\task";#"F:\Workspace\trunk\SharedCode\contiki-3.0";"F:\Workspace\trunk\SharedCode\contiki-3.0\sys"#GENPATH:                Paths where application source and prm files can be#                         foundGENPATH=.\Sources;$(INSTALLPATH)\lib\hc12c\src;$(INSTALLPATH)\lib\hc12c\include;$(INSTALLPATH)\lib\hc12c\lib;.\Sources\user\arch;.\Sources\user\bsw;.\Sources\user\module;.\Sources\user\oop;.\Sources\user\task;F:\Workspace\trunk\SharedCode\contiki-3.0;F:\Workspace\trunk\SharedCode\contiki-3.0\sys; #OBJPATH:                Path where compiler and assembler will place object filesOBJPATH=.\bin#ABSPATH:                Path where linker will place executable fileABSPATH=.\bin#TEXTPATH:               Path where linker will place map file and compiler#                        disassembly listing file and dependency file.TEXTPATH=.\bin # The name of the dependency list file. Here the compiler itself updates the# make file!DEP_LIST_FILE=$(PROJECT).dep  #ENVOPTIONS:             Command line options to set environment variables.ENVOPTIONS=-ENV"GENPATH=$(GENPATH)" -ENV"OBJPATH=$(OBJPATH)" \   -ENV"ABSPATH=$(ABSPATH)" -ENV"TEXTPATH=$(TEXTPATH)"# Here there are some special options to select the object file format for# compiler/assembler/linkerCC_OBJ_FORMAT=-F2 AA_OBJ_FORMAT=-F2 LL_OBJ_FORMAT=-Fe # Compiler settings, C and C++ options.# Short description about the options used (you may adapt this options to your# own need):#  -Lasm:    Produce listing file#  -Lm:      Generate dependency information#  -LmCfg:   Configuration options for -Lm: m=write path of main file, i=write#            path of included files, u=update information#  -D:       Add preprocessor define, here it defines the target derivative name#  -WmsgFob: Option to configure the message output format. Here we changed the#            format so that the column number is written too#  -C++f:    Use full C++ mode for C++ filesCC=$(INSTALLPATH)\prog\cHC12.exe CCFLAGS_COMMON= $(CC_OBJ_FORMAT) -Lasm -Lm=$(DEP_LIST_FILE) -WmsgNu=abcet \                 -I$(INCLUDEPATH) -LmCfg=ilmu $(ENVOPTIONS) CCFLAGS=$(CCFLAGS_COMMON) -CpuHCS12 -DPPAGE_ADDR=0x15 -Ms -Cf CPPFLAGS= $(CCFLAGS_COMMON) -C++f # Assembler settings# Short description about the options used (you may adapt this options to your# own need):AA=$(INSTALLPATH)\prog\aHC12.exe  $(AA_OBJ_FORMAT) -WmsgNu=abcet $(ENVOPTIONS) AAFLAGS= -CpuHCS12 -Ms # linker settings# Short description about the options used (you may adapt this options to your# own need):#  -M:       Generate map file (overwrites the optional MAPFILE command in the#            linker parameter file#  -O:       Name of the output file. Overwrites the optional one specified in the#            linker parameter file#  -Add:     The list of object/library files specified here is linked to the#            application (together with the ones specified in the linker parameter#            file)LL=$(INSTALLPATH)\prog\linker.exe LLFLAGS=  -M -O$(PROJECT).abs -WmsgNu=abcet -Add($(ALL_OBJ_FILES) $(ADD_OBJECTS)) \           $(LL_OBJ_FORMAT) $(ENVOPTIONS) # burner settings, only used for S-Record, Intel HEX or binary output files# Short description about the options used (you may adapt this options to your# own need):#  OPENFILE: Creates/opens the destination file#  format:   Format of the file, here it is motorola S-Record#  origin:   Start address from where to copy, here begin of memory (address zero)#  len:      Set to maximum, that is the whole application#  busWidth: Set to one, thus no splitting between different eeproms#  SENDBYTE: Starts generation of the outputBB=$(INSTALLPATH)\prog\burner.exe BBFLAGS=   $(ENVOPTIONS) \   OPENFILE "$(PROJECT).s19" \   format = motorola \   origin = 0x0000 \   len = 0xffffffff \   busWidth = 1 \   SENDBYTE 1 "$(PROJECT).abs"# libmaker settings, only used for libraries# Short description about the options used (you may adapt this options to your# own need):LM=$(INSTALLPATH)\prog\libmaker.exe LMFLAGS= $(ENVOPTIONS) -NoPath -Cmd"$(ALL_OBJ_FILES) $(ADD_OBJECTS) = $(PROJECT).lib"################################################################################### from here you don't need to adapt the automake file################################################################################### build object file list with search and replace operationCPP_OBJ_FILES = $(SOURCE_FILES:.cpp=.o) CXX_OBJ_FILES = $(CPP_OBJ_FILES:.cxx=.o) C_OBJ_FILES   = $(CXX_OBJ_FILES:.c=.o) S_OBJ_FILES   = $(C_OBJ_FILES:.s=.o) ALL_OBJ_FILES = $(S_OBJ_FILES:.asm=.o) ###################################### rules###################################### top targetall: $(PROJECT).$(BUILD_TARGET_EXT)   echo *** $(PROJECT) is up to date. *** # this targets enforces a rebuild:# 1) delete the dependency info file (may contain outdated information)# 2) call a second maker process to build the target again, with following options:#    $(MAKEFILE):  Make file, which is this file#     -Prod:        Project file with all other settings#     -WmsgVrb:     Use verbose mode, so we know what is going on#     -D:           Pass through macro variables we got from the invocation line#                   directly (INSTALLPATH)#     -ViewMin:     Run as iconified application#     -Mkall:       Make the target without checking for dependency datesrebuild:   -del $(DEP_LIST_FILE)   -del $(TEXTPATH)\$(DEP_LIST_FILE)   $(INSTALLPATH)\prog\maker.exe $(MAKEFILE) $(ENVOPTIONS) -WmsgVrb \               -D(INSTALLPATH=$(INSTALLPATH)) -ViewMin -mkall   echo "*** rebuild done ***" $(PROJECT).abs: $(LINKFILE) $(MAKEFILE) $(ALL_OBJ_FILES) $(ADD_OBJECTS)   $(LL) $(LLFLAGS) $(LINKFILE)   $(BB) $(BBFLAGS)  $(PROJECT).lib: $(MAKEFILE) $(ALL_OBJ_FILES) $(ADD_OBJECTS)   $(LM) $(LMFLAGS) # various rules how to build an object file from a source file.c.o:   $(CC) $(CCFLAGS) $*.c  .cpp.o:   $(CC) $(CPPFLAGS) $*.cpp  .cxx.o:   $(CC) $(CPPFLAGS) $*.cxx  .asm.o:   $(AA) $(AAFLAGS) $*.asm  .s.o:   $(AA) $(AAFLAGS) $*.s ########################################################dependency section, generated/updated by the compiler####################################################### INCLUDE $(DEP_LIST_FILE)

 

can anyone help on this ?

 

thanks,

Pamis

Labels (1)
0 Kudos
Reply
1 Solution
1,611 Views
pamis
Contributor II

...I find the reason. I haven't revise the GENPATH variable in build.bat file.

View solution in original post

0 Kudos
Reply
2 Replies
1,612 Views
pamis
Contributor II

...I find the reason. I haven't revise the GENPATH variable in build.bat file.

0 Kudos
Reply
1,611 Views
pamis
Contributor II
############################## Auto-make file: default.mak############################## Following variables should be updated to reflect you current project settings.# PROJECT:                                      Project name. Name of the final absolute/S19/library file,#                       without path informationPROJECT=Project # SOURCE_FILES:                                 All C/C++/ASM files (without path)SOURCE_FILES=datapage.c Start12.c main.c mc9s12vr48.c clock.c etimer.c process.c stimer.c timer.c Hal.c Hil.c Anti-pinch.c Diagnose.c SafeRank.c MotorClass.c Debug.c Motor.c Operation.c RealtmSt.c Skylight.c # ADD_OBJECTS:                                  Additional object/library files to link withADD_OBJECTS=ansisf.lib # INSTALLPATH:          Path where tools are installed (root installation#                       directory). If called from build.bat, INSTALLPATH#                       is through -D option.#                       Remove comment below and adjust path if INSTALLPATH is not#                       set on make invocation line#INSTALLPATH=C:\Freescale\CodeWarrior_HC12# LINKFILE:             Linker parameter file to be usedLINKFILE=.\prm\project.prm# MAKEFILE:             Name of this make fileMAKEFILE=makefile.mak # define here if you want to build a absolute file (abs) or a library (lib)BUILD_TARGET_EXT=abs#BUILD_TARGET_EXT=lib#INCLUDEPATH:           Paths where application or system include files can be#                       found.INCLUDEPATH="$(INSTALLPATH)\lib\hc12c\include"#".\Sources\user\arch";#".\Sources";#".\Sources\user\bsw";".\Sources\user\module";".\Sources\user\oop";".\Sources\user\task";#"F:\Workspace\trunk\SharedCode\contiki-3.0";"F:\Workspace\trunk\SharedCode\contiki-3.0\sys"#GENPATH:                Paths where application source and prm files can be#                         foundGENPATH=.\Sources;$(INSTALLPATH)\lib\hc12c\src;$(INSTALLPATH)\lib\hc12c\include;$(INSTALLPATH)\lib\hc12c\lib;.\Sources\user\arch;.\Sources\user\bsw;.\Sources\user\module;.\Sources\user\oop;.\Sources\user\task;F:\Workspace\trunk\SharedCode\contiki-3.0;F:\Workspace\trunk\SharedCode\contiki-3.0\sys; #OBJPATH:                Path where compiler and assembler will place object filesOBJPATH=.\bin#ABSPATH:                Path where linker will place executable fileABSPATH=.\bin#TEXTPATH:               Path where linker will place map file and compiler#                        disassembly listing file and dependency file.TEXTPATH=.\bin # The name of the dependency list file. Here the compiler itself updates the# make file!DEP_LIST_FILE=$(PROJECT).dep  #ENVOPTIONS:             Command line options to set environment variables.ENVOPTIONS=-ENV"GENPATH=$(GENPATH)" -ENV"OBJPATH=$(OBJPATH)" \   -ENV"ABSPATH=$(ABSPATH)" -ENV"TEXTPATH=$(TEXTPATH)"# Here there are some special options to select the object file format for# compiler/assembler/linkerCC_OBJ_FORMAT=-F2 AA_OBJ_FORMAT=-F2 LL_OBJ_FORMAT=-Fe # Compiler settings, C and C++ options.# Short description about the options used (you may adapt this options to your# own need):#  -Lasm:    Produce listing file#  -Lm:      Generate dependency information#  -LmCfg:   Configuration options for -Lm: m=write path of main file, i=write#            path of included files, u=update information#  -D:       Add preprocessor define, here it defines the target derivative name#  -WmsgFob: Option to configure the message output format. Here we changed the#            format so that the column number is written too#  -C++f:    Use full C++ mode for C++ filesCC=$(INSTALLPATH)\prog\cHC12.exe CCFLAGS_COMMON= $(CC_OBJ_FORMAT) -Lasm -Lm=$(DEP_LIST_FILE) -WmsgNu=abcet \                 -I$(INCLUDEPATH) -LmCfg=ilmu $(ENVOPTIONS) CCFLAGS=$(CCFLAGS_COMMON) -CpuHCS12 -DPPAGE_ADDR=0x15 -Ms -Cf CPPFLAGS= $(CCFLAGS_COMMON) -C++f # Assembler settings# Short description about the options used (you may adapt this options to your# own need):AA=$(INSTALLPATH)\prog\aHC12.exe  $(AA_OBJ_FORMAT) -WmsgNu=abcet $(ENVOPTIONS) AAFLAGS= -CpuHCS12 -Ms # linker settings# Short description about the options used (you may adapt this options to your# own need):#  -M:       Generate map file (overwrites the optional MAPFILE command in the#            linker parameter file#  -O:       Name of the output file. Overwrites the optional one specified in the#            linker parameter file#  -Add:     The list of object/library files specified here is linked to the#            application (together with the ones specified in the linker parameter#            file)LL=$(INSTALLPATH)\prog\linker.exe LLFLAGS=  -M -O$(PROJECT).abs -WmsgNu=abcet -Add($(ALL_OBJ_FILES) $(ADD_OBJECTS)) \           $(LL_OBJ_FORMAT) $(ENVOPTIONS) # burner settings, only used for S-Record, Intel HEX or binary output files# Short description about the options used (you may adapt this options to your# own need):#  OPENFILE: Creates/opens the destination file#  format:   Format of the file, here it is motorola S-Record#  origin:   Start address from where to copy, here begin of memory (address zero)#  len:      Set to maximum, that is the whole application#  busWidth: Set to one, thus no splitting between different eeproms#  SENDBYTE: Starts generation of the outputBB=$(INSTALLPATH)\prog\burner.exe BBFLAGS=   $(ENVOPTIONS) \   OPENFILE "$(PROJECT).s19" \   format = motorola \   origin = 0x0000 \   len = 0xffffffff \   busWidth = 1 \   SENDBYTE 1 "$(PROJECT).abs"# libmaker settings, only used for libraries# Short description about the options used (you may adapt this options to your# own need):LM=$(INSTALLPATH)\prog\libmaker.exe LMFLAGS= $(ENVOPTIONS) -NoPath -Cmd"$(ALL_OBJ_FILES) $(ADD_OBJECTS) = $(PROJECT).lib"################################################################################### from here you don't need to adapt the automake file################################################################################### build object file list with search and replace operationCPP_OBJ_FILES = $(SOURCE_FILES:.cpp=.o) CXX_OBJ_FILES = $(CPP_OBJ_FILES:.cxx=.o) C_OBJ_FILES   = $(CXX_OBJ_FILES:.c=.o) S_OBJ_FILES   = $(C_OBJ_FILES:.s=.o) ALL_OBJ_FILES = $(S_OBJ_FILES:.asm=.o) ###################################### rules###################################### top targetall: $(PROJECT).$(BUILD_TARGET_EXT)   echo *** $(PROJECT) is up to date. *** # this targets enforces a rebuild:# 1) delete the dependency info file (may contain outdated information)# 2) call a second maker process to build the target again, with following options:#    $(MAKEFILE):  Make file, which is this file#     -Prod:        Project file with all other settings#     -WmsgVrb:     Use verbose mode, so we know what is going on#     -D:           Pass through macro variables we got from the invocation line#                   directly (INSTALLPATH)#     -ViewMin:     Run as iconified application#     -Mkall:       Make the target without checking for dependency datesrebuild:   -del $(DEP_LIST_FILE)   -del $(TEXTPATH)\$(DEP_LIST_FILE)   $(INSTALLPATH)\prog\maker.exe $(MAKEFILE) $(ENVOPTIONS) -WmsgVrb \               -D(INSTALLPATH=$(INSTALLPATH)) -ViewMin -mkall   echo "*** rebuild done ***" $(PROJECT).abs: $(LINKFILE) $(MAKEFILE) $(ALL_OBJ_FILES) $(ADD_OBJECTS)   $(LL) $(LLFLAGS) $(LINKFILE)   $(BB) $(BBFLAGS)  $(PROJECT).lib: $(MAKEFILE) $(ALL_OBJ_FILES) $(ADD_OBJECTS)   $(LM) $(LMFLAGS) # various rules how to build an object file from a source file.c.o:   $(CC) $(CCFLAGS) $*.c  .cpp.o:   $(CC) $(CPPFLAGS) $*.cpp  .cxx.o:   $(CC) $(CPPFLAGS) $*.cxx  .asm.o:   $(AA) $(AAFLAGS) $*.asm  .s.o:   $(AA) $(AAFLAGS) $*.s ########################################################dependency section, generated/updated by the compiler####################################################### INCLUDE $(DEP_LIST_FILE)
0 Kudos
Reply