你好,我正在使用CW11编写MC9S12ZVML31的程序,碰到了一个问题
假如采用这样编程:
方法一:
const char a[]="\nUVWAveInitOver!";
UartSendStr(UART1,a);
void UartSendStr(unsigned char UartNum,const char *Point)
{
while(*Point!=0)
{
UartSend(UartNum,*Point);
Point++;
}
}
编译出来的MAP文件
.init 54 R 0xFE8000 0xFE8035 ROM
.startData 27 R 0xFE8036 0xFE8050 ROM
.rodata 144 R 0xFE8054 0xFE80E3 ROM **********************
.text 16564 R 0xFE80E4 0xFEC197 ROM
.copy 2288 R 0xFEC198 0xFECA87 ROM
.stack 512 R/W 0x1000 0x11FF RAM
ptuTrigE 40 R/W 0x1200 0x1227 RAM
adcLists 128 R/W 0x1228 0x12A7 RAM
.data 2164 R/W 0x12A8 0x1B1B RAM **********************
方法2:
UartSendStr(UART1,"\nUVWAveInitOver!");
void UartSendStr(unsigned char UartNum,const char *Point)
{
while(*Point!=0)
{
UartSend(UartNum,*Point);
Point++;
}
}
编译出来的MAP文件
.init 54 R 0xFE8000 0xFE8035 ROM
.startData 27 R 0xFE8036 0xFE8050 ROM
.rodata 124 R 0xFE8054 0xFE80CF ROM **********************
.text 16542 R 0xFE80D0 0xFEC16D ROM
.copy 2308 R 0xFEC16E 0xFECA71 ROM
.stack 512 R/W 0x1000 0x11FF RAM
ptuTrigE 40 R/W 0x1200 0x1227 RAM
adcLists 128 R/W 0x1228 0x12A7 RAM
.data 2184 R/W 0x12A8 0x1B2F RAM **********************
字符串"\nUVWAveInitOver!"方法一占用.rodata即144-124=20字节 方法二占用.data即 2184-2164=20字节
问题:为什么方法2的方式占用RAM空间,别的编译器对字符串都占用.rodata空间?如何在使用方式二的情况下字符串占用.rodata空间(注:如果我采用方式一,程序的可读性就不好了。)
帮我一下,谢谢