new to codewarrior for palm os sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

new to codewarrior for palm os sdk

866 Views
doggy
Contributor I

hi, usually i am programming microcontrollers in basic, and am just starting to pick up on C,, but for now i got this codewarrior &palm OS sdk, but i am having problems getting the code together, sofar I have been able to make a RSC file with the PilRC and the h header and rsrc file(whatever that is)

 

i think, i am importing it correctly, but I am having problems getting in the source code( I think), can i get a sample mcp file, all i need is a working form and some working buttons, as a sample template for myself??

 

(i hope im in the right place!)

Labels (1)
0 Kudos
Reply
2 Replies

673 Views
J2MEJediMaster
Specialist I

The Palm OS version of Codewarrior has not be supported by Freescale for some years now. Sorry.

 

---Tom

 

0 Kudos
Reply

673 Views
doggy
Contributor I

that is OK, i think you may be able to help anyway, right now i have the H file and rsc files attached that integrate the code, but I am having problems writing the source.c code,.   right now I only have 3 forms with a button on each, all i need to do is to create a loop that will go to the next form when the button is pressed,   

 

any help could be helpful!

thnx

0 Kudos
Reply