how to run dsp as stand alone board and can we run two boards at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to run dsp as stand alone board and can we run two boards at the same time

2,349 Views
siri
Contributor I
Hello

I have two questions.

1. How to run dsp as stand alone station, if possible ? meaning once code is downloaded on to the board there should not be any connection between the host computer and itself

2.Is there a way to run two dsp boards at the same time ?

If someone could answer these questions, I will be very grateful..


Thanks,
sirisha


Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

635 Views
siri
Contributor I
Hello

Thanks alot for your response. I have one more question, which is not very clear to me at all is:

what do the CPU configuration sdm, idm mean ?? and xROM, and pROM ??

I really appreciate your help .

Sirisha
0 Kudos
Reply

635 Views
trytohelp
NXP Employee
NXP Employee
sdm: small memory
ldm: large memory
 
For DSP there are 2 memories: DATA and CODE
DATA  is defined by x
CODE is defined by p
For each memory there are:
 External, flash, ram and for DATA IO.
So by this way xRAM is the RAM from DATA and pRAM is the RAM from CODE
 
for details I recommend you to create a project with Processor Expert.
Under Processor Expert menu you can open the Memory Map.
Some information is given in the cmd file too.
 
Hope this will help you.
Pascal
0 Kudos
Reply

635 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
You can run a dsp ins stand alone mode.
By default the application  will re-start after a hardware reset or power off/on.
 
To do that we recommend you to use the target wizard to create your application.
In the project setting select the target named "ldm pROM_xRAM".
 
For the second question.
What do you want to do ?
Debug 2 applications with the same PC on 2 DSP boards ?
 
Regards
Pascal
0 Kudos
Reply