header files of jendefs.h not present

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

header files of jendefs.h not present

1,247 Views
dheerajsawant
Contributor V

Hello friends, 

i am using beyond studio for first time. i have install JN-SW-4141 and JN-SW-4165.

Try to import example like device bulb or JN516x Customer Module Evaluation Tool. (JN-AN-1172).

all steps perform well except when i try to build. it show error on include files which are listed below.

1)jendegs.h

2)AppHardwareApi.h

on this files it shows error. i recheck this files again in c drive. but i did'n see. 

why these header files are not already included?

because in every example this files are present.

am i wrong at some place please help me. 

0 Kudos
Reply
1 Reply

838 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi  Dheeraj,

The errors you are seeing is Eclipse not being able to resolve various variable and functions within the SDK.

But you can compile the Application note successfully.

Are you seeing errors in the Console section?

Best Regards,

Mario

0 Kudos
Reply