goto command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

goto command

1,965件の閲覧回数
ElliottKevin
Contributor I
dear warriors
 
could you say me how i can use the go to command in command line of debug window. for instance goto command make your codes execute untill given label.
 
goto port_init
   ...
   ..
  ...
port_init
 
when i used this command in command window of debug, there is an eror message that "goto command can only be used on command window"
 
do you have any idea? this command is very important to test code execution.
best regards
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,438件の閲覧回数
CrasyCat
Specialist III

Hello

 

- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?


To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.

 

Are you using the goto command within a debug command file?

You cannot use the goto command in the command window itself. You can only use it within a command file.

 

CrasyCat

0 件の賞賛
返信

1,438件の閲覧回数
ElliottKevin
Contributor I
0 件の賞賛
返信