does PC8013-61540-120443 cpu have problems for the demoboard of 56F8013

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does PC8013-61540-120443 cpu have problems for the demoboard of 56F8013

1,304 Views
duck
Contributor I
Hi:
 
I used CW7.3 and now CW8.0(special edition), use beans to setup ADC interrupt,PWM, and TMR. the problem that I am having right now is no matter how i setup beans, it just does not go into adc or pwm interrupts. however if i write code without PE beans (which is combination of c and assemble), it actually can go into pwm interrupt. so I want to know that if this PC8013 has some problem on PE initialization? otherwise I do not know why it can not go into adc interrupt.

 

Thanks!!


Labels (1)
Tags (1)
0 Kudos
1 Reply

201 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
Did you tried the example delivered on the installation ?
There is an example using the PWM build for the 8013 demo board.
Can you try it ?
  \Stationery\Processor_Expert_Examples\DemoApplications\56F8013_DemoBoard\PWM_Example
There is another example using the ADC bean for the 801x board.
Can you try it ?
  \Stationery\Processor_Expert_Examples\DemoApplications\HWBeans\56F801x\ADC
 
If you still meet the problem I suggest you to report your problem to our Technical Support team.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
Pascal
0 Kudos