calling functions from external files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

calling functions from external files

ソリューションへジャンプ
2,388件の閲覧回数
antony_GB
Contributor I

Hello everybody,

 

                        Please excuse my newb question. The problem I am having is that I can't seem to call functions defined in external files. At the moment, in order to try and do so, I am using the following structure:

 

In "Main.c"

---------------------------------------------------------------

#include "header_file.h"

 

/*call function*/

<r-type> <function_name> ();

---------------------------------------------------------------

 

In "header_file.h"

--------------------------------------------------------------

/*function prototype*/

<r-type> <function_name> (<p-type> <p-name>)

--------------------------------------------------------------

 

In "file_containing_function.c"

-------------------------------------------------------------

/*define function*/

<r-type> <function_name> (<p-type> <p_name>)

{

       some_code;

}

-------------------------------------------------------------

-------------------------------------------------------------

 

The main.c file obviously already exists, however I have added both the "header_file.h" containing the function prototype; and the "file_containing_function.c" which defines my function to my project. Can somebody please explain to me why when in debug mode, I cannot view the 'stack crawl window' step through the function in the external file. It simply seems to bypass the function call altogether.

 

Thanks for your help.  

ラベル(1)
0 件の賞賛
返信
1 解決策
1,705件の閲覧回数
CrasyCat
Specialist III

Hello

 

First I assume there is a typo in your initial post. Content of main.c should read as:

 

In "main.c"

---------------------------------------------------------------

#include "header_file.h"

 

<r-type>  retval;

 

/*call function*/

retVal =  <function_name> ();

---------------------------------------------------------------

 

Then next question is which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
   To retrieve that info:
      - Start CodeWarrior
      - Select Help -> About Freescale CodeWarrior
      - Click on "Install Products"
      - CodeWarrior version used is displayed on top in the Installed Products dialog.

 

Finally did you enable generation of debug information on file_containing_function.c?

Please check FAQ-27442 on www.freescale.com for more details on how to figure that out.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,706件の閲覧回数
CrasyCat
Specialist III

Hello

 

First I assume there is a typo in your initial post. Content of main.c should read as:

 

In "main.c"

---------------------------------------------------------------

#include "header_file.h"

 

<r-type>  retval;

 

/*call function*/

retVal =  <function_name> ();

---------------------------------------------------------------

 

Then next question is which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
   To retrieve that info:
      - Start CodeWarrior
      - Select Help -> About Freescale CodeWarrior
      - Click on "Install Products"
      - CodeWarrior version used is displayed on top in the Installed Products dialog.

 

Finally did you enable generation of debug information on file_containing_function.c?

Please check FAQ-27442 on www.freescale.com for more details on how to figure that out.

 

CrasyCat

0 件の賞賛
返信
1,705件の閲覧回数
antony_GB
Contributor I

Thanks CrasyCat for correcting my syntax. Problem solved.

0 件の賞賛
返信