What options do I have now that I am using a Windows 10 64 bit computer and have the classic CW IDE with USB Dongle?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What options do I have now that I am using a Windows 10 64 bit computer and have the classic CW IDE with USB Dongle?

922件の閲覧回数
paulrees
Contributor I

I am told the USB Dongle is no longer supported with the classic Code Warrior IDE when used on either a Windows 7 or Windows 10 64 bit computer.

 

So, exactly what do I need to do to use the classic Code Warrior IDE? I don't believe there should be any cost to my  Company associated with any licencing changes.

ラベル(1)
0 件の賞賛
返信
1 返信

773件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Paul,

our recommendation is to rehost the license file to the DISK/HOST ID.

Please see this link answer from Pascal

https://community.nxp.com/thread/350063 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信