I have to make upgrades to old software done on an Window XP system. I have successfully installed virtual PC and the newer version of CodeWarrior 6.3. (I previously used 5.1.) Although the code warrior software runs on the virtual pc, I cannot connect to my target board - a DEMO908GZ60. I believe I have set all the jumpers correctly to enter the MON08 mode, and the loader program indicates that the COM1 port is opened (7200 baud with a Class 3 device) There is no connection made. The connection status reads NN(Port?)NNN. I have also checked the box to ignore the security protocol. Does anyone know if there are special considerations while programming the target board in virtual PC? This worked fine before on the XP system. I don't know what I'm doing wrong now.