Hello
I am able to use V8 without any trouble in CodEwarrior for HC12 V5.1.
I do not have PC-Lint V9 installed on my system so I cannot check with that version.
I noticed something strage though. In your Lint command line you are using co-mwe_base.lnt instead of co-mwhc12.lnt.
Is the file co-mwhc12.lnt available in your installation Lint\lnt\CodeWarrior folder?
If you are still unable to get it to work, I may recommend you to submit a service request through our on line support
web site.
Click here to submit a service request.
Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.
Attach the generated .zip file to the SR.
CrasyCat