USBTAP installation problem for codewarrior version 7.0 of 568000E

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USBTAP installation problem for codewarrior version 7.0 of 568000E

跳至解决方案
2,344 次查看
admin
Specialist II
I need to installation codewarrior version 7 for 56800E, because to maintain our old project which transfer from our partner. this project coded by codewarrior version 7.
 
when I installed the codewarrior 7 which download from freescale website, but I can't find the USB TAP connection Item in the "Remote Connection" tap.
 
when I install the "ROHS USB TAP Update.ext",  but some problem appears. It says that:"Setup was unable to find the qulified installation of codewarrior tools on your system. Please select the location below,and press "Next" to start the file update."
 
I had choose many many different location which my codewarrior 7.0 installed, but always can't go ahead.
 
who can give me some advice to fix this USB  TAP connection for codewarrior 7.0 of 56800E.
 
Thanks
 
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
810 次查看
stalisman
Contributor III

Hi Xiaogang

 

I had similar problems when I installed v7.1 alongside v6.3.

 

The installations share a folder:  C:\Documents and Settings\YOUR LOGIN NAME\Local Settings\Application Data\Metrowerks.

 

This folder is updated each time you launch and IDE and it can get confused.

 

I deleted the contents of this folder and then relaunched v7.1 and the USB Tap option reappeared.

 

It is a pain that you have to redo your project settings but it worked for me.

 

 

Good luck

 

Regarding the "ROHS USB TAP Update.exe" error it's almost certainly a bug in the Update executable itself, and best ignored as clearing out the above folder will most probably solve your problem.

 

Message Edited by stalisman on 2009-07-24 11:16 AM

在原帖中查看解决方案

0 项奖励
回复
1 回复
811 次查看
stalisman
Contributor III

Hi Xiaogang

 

I had similar problems when I installed v7.1 alongside v6.3.

 

The installations share a folder:  C:\Documents and Settings\YOUR LOGIN NAME\Local Settings\Application Data\Metrowerks.

 

This folder is updated each time you launch and IDE and it can get confused.

 

I deleted the contents of this folder and then relaunched v7.1 and the USB Tap option reappeared.

 

It is a pain that you have to redo your project settings but it worked for me.

 

 

Good luck

 

Regarding the "ROHS USB TAP Update.exe" error it's almost certainly a bug in the Update executable itself, and best ignored as clearing out the above folder will most probably solve your problem.

 

Message Edited by stalisman on 2009-07-24 11:16 AM
0 项奖励
回复