USB Tap noise sensitivity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Tap noise sensitivity

1,827 次查看
Oppie
Contributor I

We were having several problems with a spontaneous target reset or loss of communication between the target and USB Tap when debugging a DSP56F8357. This became very obvious when we had one engineer performing ESD (electro-static discharge) testing on a system across the room from another engineer debugging with a USB TAP.  Quite often, on a discharge event, the target system would reset. Very strange since the two projects were on different benches and served by different electrical systems.

 

By adding a ground lug to the USB tap case and connecting it with a faston terminal and 18AWG wire to the target earth ground, all the reset and communication problems went away. We were shooting 10KV sparks repetitively to a system in close proximity (that would have made Marconi proud) with no USB Tap problems. Before the addition of case ground, even 4KV would cause problems from a further distance.

 

This would suggest that something is either weakly terminated or floating inside the Tap's case or that the case itself is not grounded to anything internal.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

663 次查看
trytohelp
NXP Employee
NXP Employee
Hi,
 
I suggest you to log your request to the Freescale CRM system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request to create a new one or Manage Existing Service Request.
  - You will come to a login page.
  - You can submit your request through the web from there or view the activities of a SR.
We should contact the development team regarding this USBTap question.
 
Regards
Pascal
0 项奖励
回复