USB Tap Err, CW ver 7 and also 8, Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Tap Err, CW ver 7 and also 8, Error

1,643 次查看
san_jon
Contributor I

Hi,

 

I have been using USB TAP successfully from last 2 years.

 

Because of some other project, I had not used the USB TAP for 3 weeks. 

 

Now while downloading Code to EVM or Application Board, I get various errors saying

 

1. Core not responding

 

2. Unable to Write to Flash

 

3. The Flash is locked

- In this case i went to Debug -> 56800E -> Unlock Flash, and tried again, in this case i get error mentioned in 2.

 

USB Drivers seems allright, as it shows under windows device drivers, also i installed update of USB TAP.

 

and i have captured comm data using "show com" in ccs window. 

 

Any help / direction to solve this problem would be helpful, 

thanks in advance.

 

San

-------------------------------------------------------------------

 

Show commands turned on
Received  CMD_CONFIG_CHAIN. count = 0
command done - Ok
Connection #1 accepted from localhost at Wed Apr 21 15:46:51 2010
Received  CMD_CHECK_MIN_VERSION
command done - Ok
Received  CMD_AVAILABLE_CONNECTIONS
command done - Ok
Received  CMD_DELETE_CC
command done - Ok
Received  CMD_SETUP_CC.CC = utap:
command done - Ok
Received  CMD_CONFIG_CHAIN. count = 1
    core 0: HawkV2
Available USB TAPs:
08340336
Opening connection to USB TAP 08340336
0: USB TAP (JTAG) (utap:smileyhappy: Loader software ver. {1.6}
Sending code to USB TAP - please wait
Sending CMD_SERVER_ALIVE
Sending CMD_SERVER_ALIVE
Available USB TAPs:
08340336
Opening connection to USB TAP 08340336
Received an unknown command 46
USB TAP command done - Ok
USB TAP command done - Ok
Received  CMD_RESET_TO_DEBUG
USB TAP command done - Ok
Received  CMD_SET_MAX_TCK. chain_pos = 0,khz = 5000
USB TAP command done - Ok
Received  CMD_CONFIG_TEMPLATE. chain_pos = 0, index = 3, value = 1
USB TAP command done - Ok
Received  CMD_CONFIG_TEMPLATE. chain_pos = 0, index = 4, value = 1000
USB TAP command done - Ok
Received  CMD_WRITE_REG. chain_pos = 0, index = 23, count = 1
    register 23 = 0xcccc
USB TAP command done - Ok
Received  CMD_READ_REG. chain_pos = 0, index = 0, count = 51
USB TAP command done - Ok
Received  CMD_READ_REG. chain_pos = 0, index = 52, count = 5
USB TAP command done - Core not in debug
Received  CMD_CONFIG_CHAIN. count = 0
USB TAP command done - Ok
Connection #1 from localhost closed at Wed Apr 21 15:46:58 2010

-----------------------------------------------------------------

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

730 次查看
J2MEJediMaster
Specialist I

What has changed in the past three weeks wth the setup?

 

Are you using a new board with the old setup?

 

Has something been installed on the system since the last time it was used?

 

Was a cable changed?

 

---Tom

0 项奖励
回复