The use of ADC module of MC9S12ZVLS32.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The use of ADC module of MC9S12ZVLS32.

1,821 次查看
robin_jiang
Contributor I

Hello I want to obtain some sample codes for the use of ADC module of MC9S12ZVLS32.  

标签 (1)
1 回复

1,756 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tianhao Jiang

I suggest you refer:

AN5168 Using the ADC Module in S12ZVM

https://www.nxp.com/docs/en/application-note/AN5168.pdf 

http://www.nxp.com/files/microcontrollers/doc/app_note/AN5168SW.zip 

Both S12ZVM and S12ZVL are ADC12B_LBA module. So you can refer it for your S12ZVL device.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------