Setting up the JTAG connector for a MC56F8006demo board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting up the JTAG connector for a MC56F8006demo board

ソリューションへジャンプ
4,054件の閲覧回数
lincharles
Contributor I

Hi all,

 

I am trying to download applications from CodeWarrior 56800/E V8.2.3 onto a MC56F8006demo board via a parallel-to-JTAG converter. I am running CodeWarrior on a 32-bit Vista computer. Whenever I press the debug button, I receive an error of "cssprotocolplugin: unknown protocol error". I have tried the following tips from a previous thread, http://forums.freescale.com/freescale/board/message?board.id=CWDSPCOMM&message.id=697&query.id=11033..., but the error persists.

 

  - "Enable Legacy Plug and Play" is checked for my parallel port

  - The parallel port registration key, winxp2.reg is added

  - The mode of my parallel port is set to bi-directional

  - The address of the parallel port is set using commands "config cc Parallel:0x0378" and "config save"

  - The voltage coming out of my parallel port from my desktop is 5v

 

 

The log of my session says:

check_min_version(serverh=0,*version)
  api version: 00000004 00000005
config_chain(serverh=0,cc=0,count=1,*devlist,*generic)
  devlist: Holo
reset_to_debug(serverh=0,cc=0)
  ERROR(39): Subcore error encountered during multicore operation

 

Is there any other configuration need to be done before I can use a JTAG connector to download applications?

 

Thanks in advance,

 

Charles

 

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,422件の閲覧回数
J2MEJediMaster
Specialist I

Most of the suggestions you followed were for Windows XP systems. I do not know what the situation is for Vista, but I know how that Vista does handle drivers a bit differently.

 

You seem to have done all of the right things, so the only thing I can suggest is that you try the set-up on a system running Windows XP. I know, that is not the best suggestion given the lack of resources these days, but it would at least point out if the Vista was the culprit.

 

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,423件の閲覧回数
J2MEJediMaster
Specialist I

Most of the suggestions you followed were for Windows XP systems. I do not know what the situation is for Vista, but I know how that Vista does handle drivers a bit differently.

 

You seem to have done all of the right things, so the only thing I can suggest is that you try the set-up on a system running Windows XP. I know, that is not the best suggestion given the lack of resources these days, but it would at least point out if the Vista was the culprit.

 

---Tom

0 件の賞賛
返信
1,422件の閲覧回数
GregM
Contributor I

Honestly, is the accepted solution to this problem to uninstall Vista & install XP!?!

 

I'm having the same issue. It seems that no matter what address I point the command converter to, the error comes back as "ERROR(39): Subcore error encountered during multicore operation". 

 

What does that error actually mean? Can we not find the root of the problem and have it fixed for good?

 

Cheers,

Greg 

0 件の賞賛
返信
1,422件の閲覧回数
lincharles
Contributor I

 

 

I tried running on an XP computer and everything work just fine now. Thanks for your assistance Tom.

0 件の賞賛
返信
1,422件の閲覧回数
J2MEJediMaster
Specialist I

I scouted around the forums, and found some more information on parallel port solutions, which may be of help. The thread is:

 

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&thread.id=6144

0 件の賞賛
返信