Problem with ADC usage...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with ADC usage...

1,551 次查看
Kanthi
Contributor II

Hello Pascal,

    I am using the 56F8356 developement environment, I have peculiar problem with the ADC usage.

 I wait in a while loop for ADC conversion to get over. But the program always stays there.

 

   I am facing this problem after introducing new PWM and Decoder interrupts. I am not using any SYNCH Signal, its just the Software "START" conversion.

 

  Example of my program:

 

       GET_ADCA_OUTPUT()

{

      while( ADCA Conversion is Over)

        { 

          wait...

        }

       Return the output values..

}

 

Get_ADCB_OUTPUT()

{

      while( ADCB Conversion is Over)

        { 

          wait...

        }

       Return the output values..

}

 

If I introduce a delay factor for waiting, i am able to introduce it in only one of the loops, not in both, if i introduce in both the system is restarting.. or it stops working.

 

If I introduce a counter factor like this it works:

GET_ADCA_OUTPUT()

{

      while( ADCA Conversion is Over) && (Counter reaches zero)

        { 

          wait...

        }

       Return the output values..

}

 

Get_ADCB_OUTPUT()

{

      while( ADCB Conversion is Over)

        { 

          wait...

        }

       Return the output values..

}

 

But if i introduce a counter factor in both the loops it doesn't work..system restarts or does not function properly like this:

 

GET_ADCA_OUTPUT()

{

      while( ADCA Conversion is Over) && (Counter reaches zero)

        { 

          wait...

        }

       Return the output values..

}

 

Get_ADCB_OUTPUT()

{

      while( ADCB Conversion is Over) && (counter reaches zero)

        { 

          wait...

        }

       Return the output values..

}

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

560 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

I suggest you to log your request to the Freescale CRM system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request to create a new one or Manage Existing Service Request.
  - You will come to a login page.
  - You can submit your request through the web from there or view the activities of a SR.

Please provide us more details about the Tool version used.
To do that you must:
Start the IDE and click on Help | About Freescale CodeWarrior.
Click on Installed Products 
Provide us all info displayed.
Or you can save them in a txt file.

Can you please provide us your example reproducing the issue ?

 

Regards

Pascal

0 项奖励
回复