P1021MDS and CodeWarrier 8.8 cant connect to core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1021MDS and CodeWarrier 8.8 cant connect to core

712件の閲覧回数
PaulWalker
Contributor IV

Hi,

I am having some trouble getting up and running with a QoriQ P1021-MDS-PB evaluation board for software development. 

I have installed CodeWarrier 8.8 and SP1 to add P1021MDS board support. I have installed NetComm 0.2 driver software supplied with dev board kit.  I am also using USB TAP.

When I go through the getting started app 'hello world' the project builds ok, but when I run I get 'CCSProtocolPlugin::Could not connect to the requested core core #0' and 'core #1' errors.

What's gone wrong? Can you help?

ラベル(1)
0 件の賞賛
返信
1 返信

507件の閲覧回数
PaulWalker
Contributor IV

Worked out that the JTAG connector was round the wrong way. The plug is not keyed so will go both ways. :smileytongue:in 1 (red) must be uppermost on the board.

 

0 件の賞賛
返信