Objective-C -- Still supported?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Objective-C -- Still supported?

2,124 Views
Frotz
Contributor III
Hello!

I've been evaluating the MCU's and the CodeWarrior IDE for a software-heavy hardware project. I'm very familiar with Objective-C and find it to be a very powerful OO language. It's also very light-weight since it's a very thin layer upon C. For these reasons I'd like to use it for development on this project.

According to the "C Compliers Reference version 3.2", the objective_c pragma is available. Not having an IDE yet, nor having settled on a MCU even, I've not tested this in practise!

Is there anyone who can verify if ObjC works and if so, which MCU's it applies to?

Thank you very much,
Andre.
Labels (1)
0 Kudos
Reply
1 Reply

703 Views
trytohelp
NXP Employee
NXP Employee
Hello,
 
This problem has been reported to Support team in CRM.
The SR number 1-345621333 has been logged for this issue.
 
Pascal
TIC-CodeWarrior
0 Kudos
Reply