No headers in the source tree of Codewarrior 3.1.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No headers in the source tree of Codewarrior 3.1.1

3,181件の閲覧回数
pamplemousse_mk
Contributor I
HEllo,

I use Codewarrior 3.1.1 Personal edition for Symbian S60, evaluation version at home. When I import an MMP file (for example S60Example\HelloWorldBasic), the source tree does not show the header files in the source tree. When the "Find in files" dialog is opened, in the tab "in Project", the System Header checkbox is not available (it could not be checked) and all the includes (user and system includes) are displayed with the checkbox "Project headers" without distinction.

Curiously, when using the key binding "Go to header/source file", the header is correctly found.

At my work, we use a registered version of Codewarrior 3 and the headers are well displayed in the source tree. Is it a feature for the registered version only?

Bye.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

849件の閲覧回数
CrasyCat
Specialist III

Hello

CodeWarrior for Symbian is supported by Nokia now.

Can you post your message on Nokia forum (www.forum.nokia.com/codewarrior).?

Thanks

CrasyCat

0 件の賞賛
返信

849件の閲覧回数
pamplemousse_mk
Contributor I
Hello,

OK, I'm currently posting messages in the forum of Nokia.
Bye.
0 件の賞賛
返信