No headers in the source tree of Codewarrior 3.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No headers in the source tree of Codewarrior 3.1.1

3,209 次查看
pamplemousse_mk
Contributor I
HEllo,

I use Codewarrior 3.1.1 Personal edition for Symbian S60, evaluation version at home. When I import an MMP file (for example S60Example\HelloWorldBasic), the source tree does not show the header files in the source tree. When the "Find in files" dialog is opened, in the tab "in Project", the System Header checkbox is not available (it could not be checked) and all the includes (user and system includes) are displayed with the checkbox "Project headers" without distinction.

Curiously, when using the key binding "Go to header/source file", the header is correctly found.

At my work, we use a registered version of Codewarrior 3 and the headers are well displayed in the source tree. Is it a feature for the registered version only?

Bye.
标签 (1)
0 项奖励
回复
2 回复数

877 次查看
CrasyCat
Specialist III

Hello

CodeWarrior for Symbian is supported by Nokia now.

Can you post your message on Nokia forum (www.forum.nokia.com/codewarrior).?

Thanks

CrasyCat

0 项奖励
回复

877 次查看
pamplemousse_mk
Contributor I
Hello,

OK, I'm currently posting messages in the forum of Nokia.
Bye.
0 项奖励
回复