Must convert CodeWarrior IDE .mcp to .mak file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Must convert CodeWarrior IDE .mcp to .mak file

3,039 Views
tooldeveloper
Contributor I
I'm developing applications to automate builds and require a way to generate .mak files from the .mcp files that developers are creating and modifying. Is there a way to generate .mak files from .mcp files.
 
This is not for reverse engineering, but rather for automation. Most engineers like the Windows GUI, but for automation and releases we compile from Solaris command line and thus require .mak files - unless the Solaris compiler can actually take the .mcp files which could be another solution.
Labels (1)
0 Kudos
Reply
1 Reply

644 Views
CrasyCat
Specialist III
Hello
 Not sure which processor you are targeting.
 Basically today it is not possible to export a .mcp file into a .mak file.
CrasyCat
0 Kudos
Reply