MPC5604B: "sprintf(...)" is not possible

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604B: "sprintf(...)" is not possible

1,705 Views
Mikaza
Contributor I

Hallo together,

 

at the moment I want to transfer a serial chain of ASCII-Strings with the LIN/UART-Controller from the MPC5604B Board. So i need a function, which changes characters from binary to ASCII, so yesterday I try to use the "sprintf" - function, but without success. (stdio.h is already included).

 

How can I solve this problem? Perhaps one of you has already a solution...?

 

Best Regards and marry Christmas (and a happy new year)

Labels (1)
0 Kudos
Reply
4 Replies

1,365 Views
shri
Contributor II

void binarytoascii(uint16_t innum) {
uint16_t j1,in;
uint8_t p1,p2;
in = innum;

j1 = (in & 0x0f);
if (j1 > 9) p1 = (uint8_t)(j1 + 0x41 - 10);
else p1 = (uint8_t)(j1 +0x30);
j1 = (in & 0xf0) >> 4;
if (j1 > 9) p2 = (uint8_t)(j1 +0x41 - 10);
else p2 = (uint8_t)(j1 +0x30);
//TransmitCharacter(0x0a);
// TransmitCharacter(0x0d);
TransmitCharacter(p2);
TransmitCharacter(p1);
}

where TransmitCharacter() function looks like as below

void TransmitCharacter(uint8_t ch)
{
LINFLEX_0.BDRL.B.DATA0 = ch;                                /* write character to transmit buffer */
while (1 != LINFLEX_0.UARTSR.B.DTF) {}                 /* Wait for data transmission completed flag */
LINFLEX_0.UARTSR.R = 0x0002;                              /* clear the DTF flag and not the other flags */
}

 

set the proper baud rate of LINFLEX_0.UART

0 Kudos
Reply

1,365 Views
Mikaza
Contributor I

no hint for me?

0 Kudos
Reply

1,365 Views
Lundin
Senior Contributor IV

You could ask a programmer to write an binary to ASCII converter for you. It is such a basic task that even a beginner programmer should be able to succesfully help you out with it.

0 Kudos
Reply

1,365 Views
stanish
NXP Employee
NXP Employee

Hi Mikaza,

 

Could you perhaps post some code snippet to see how exactly you are using sprintf in this case.

 

Thanks.

Stanish

0 Kudos
Reply