Looking for 'Special Edition' of CodeWarrior for MPC8349 flash programming only

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for 'Special Edition' of CodeWarrior for MPC8349 flash programming only

547 Views
jeffgee
Contributor I

Hi

 

I'm looking for a Special Edition of CodeWarrior for MPC8349 with only the flash programming tool. I don't see any support for
the MPC8349/Power Quic family (or it's not obvious) in the Special Edition download section.

 

We don't use the development tools in this package, just the flash programming feature when our hardware gets bricked
due to a corrupt flash. I had a V8.8 install on my old XP box, but with an update to Win7, I need to do a new install.

thanks

 

Jeff

Labels (1)
0 Kudos
Reply
1 Reply

382 Views
Pavel
NXP Employee
NXP Employee

Evaluation version of CodeWarrior can be used during 30 days. There are no other limitation for using evaluation version.

Use evaluation version CodeWarrior for Flash programming on your board.

CodeWarrior 8.8 can be used on Windows 7 PC.

Install Software Patch: CW PA v8.8.6 Windows - Patch for working under Windows 7:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6121541


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply