Hello, someone have this problem??:
Link Error   : Undefined : "_d_fle"
Referenced from "IRQ_ADE_ISR" in main.c
Link Error   : Undefined : "_d_itod"
Referenced from "IRQ_ADE_ISR" in main.c
Link Error   : Undefined : "_d_utod"
Referenced from "IRQ_ADE_ISR" in main.c
Link failed.
Thanks so much!
Regards
_d_fle - is a double precision floating point compare routine. le in routine name stands for less or equal.
_d_itod - convert signed integer :smileyinfo: to double routine
_d_utod - convert unsigned integer (u) to double routine
Like suggested before, you have these options:
1) create new project and tell project wizard you want floating point.
2) add to the project required libraries
3) in your IRQ_ADE_ISR avoid using floating point.
 
					
				
		
Well, thank you so much Kef. I want to do the third option, how avoid using floating point in my IRQ_ADE_ISR routine?. It is the first time that I work with interrupt, thanks again,
Best regards!!
 
					
				
		
This file, main.c, haven´t compilation error...but I don´t know do that you say me...because yet I am inexpert in this matter
Thank
regards
You have lines like this:
if (1.1*Icorte<=get_corriente_IRMS()<=1.4*Icorte)
1) 1.1 and 1.4 are floating point numbers. To avoid FP arithmetics, you could multiply all arguments by 10. a<b<c is the same like 10a<10b<10c.
2) In C a < b < c is not the same like a < b < c in math. First a is compared to b giving logical answer true (not zero) or false (zero). Then result of a<b is compared against c. I guess this is not what you want.
Hope this is what you want:
if ( (11*Icorte <= get_corriente_IRMS()*10) && (get_corriente_IRMS()*10<=14*Icorte) )
You should make sure get_corriente_IRMS()*10 doesn't overflow, else it may not work this way.
You may fix other other occurences of 1.1 and 1.4 the same way.
 
					
				
		
Hello again!, I have solved all problems with linker... but now, when I simulate my program goes to exceptions.c....Two days ago, I enclosed my file main.c, where I define interrupt routine within this c file, but is it correct?..maybe I must define this interrupt routine out of c file...
Best regards
Thanks!!
 
					
				
		
Speaking generally, the exceptions.c file is where you specify the address of your ISR routine. In other words, this file defines the interrupt vector table for the ISRs. When an exception occurs, it first jumps to the vector table, then picks up the address of the ISR to jump to. Have you specified the name of your ISR in the appropriate location in the exceptions.c file? You might want to take a look at the CodeWarrior sample code. Usually an example of a simple interrupt routine is provided, to guide you on setting one up.
---Tom
 
					
				
		
Hello,
I am new in CodeWarrior:
-I am targeting with MCF51EM256 CPU
-My version of CodeWarrior is: Codewarrior IDE version 5.9.0 Build 2830
I´m programming with FreeRTOS kernel and I use IRQ interrupt. I don´t have any problem with linker, but when I simulate the program entry for once in the IRQ interrupts and it doesn´t entry again.
any idea?
Thanks so much..
Best regards
 
					
				
		
 CompilerGuru
		
			CompilerGuru
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		 
					
				
		
 
					
				
		
Hello I am new in CodeWarrior:
-I am targeting with MCF51EM256 CPU
-My version of CodeWarrior is: Codewarrior IDE version 5.9.0 Build 2830
I am programming with this CPU and I use vector interrupts (IRQ, vector number 64, no maskarable). I have defined within of my program (but out of routine main()) the ISR of IRQ. I compile with succes but I have any problems with the linker:
Link Error   : Undefined : "_d_fle"
Referenced from "IRQ_ADE_ISR" in main.c
Link Error   : Undefined : "_d_itod"
Referenced from "IRQ_ADE_ISR" in main.c
Link Error   : Undefined : "_d_utod"
Referenced from "IRQ_ADE_ISR" in main.c
Link failed.
What it is happens?, thanks!!
Best regards.
 
					
				
		
Thank you for your reply Lundin, but I think that my problem is in the use of IRQ interrupt, I have defined it within of my program but out of main() routine, that is correct?.
If you want see I can enclose my file.c
Thaks!!
Best regards!
Hello,
There are two different products for ColdFire target Freescale offers:
1) CodeWarrior for MCUs - supports HC(s)08 + CFv1 only
2) CodeWarrior for ColdFire - supports CFv2...v4
I'm little confused here:
The target you mentioned refers to 2) but Product name in the subject refers to option 1)
You've probably mismatched both versions. e.g. open and compile project created in 2) in CodeWarrior 1)....
Since you are targeting MCF52259 you should use CodeWarrior for ColdFire. The latest version is available here.
Stanish
HI,
Thanks for reply.
I have downloaded new Version and now i am trying to build with CW :Coldfire Architectures Version 7.1, Build 14.
I am getting same linking errors .I am aslo getng one warning "too manycommand files"
please help.
Regards,
NW