Is there a free license for CW 6.3 for assembly language ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a free license for CW 6.3 for assembly language ?

1,792 Views
philippepbo
Contributor I

Hello

After several years out of electronic design i am back and i need to set up a prototype using S08AW.

The Code warrior 6.3 is classic IDE is enough for me and i will use this IDE for evaluation of my prototype.

There is a TRAIL version available but with a 30 days limit. Since my project could take more than this i would like to know if there is any free license for CW 6.3 without C compiler ?

ThX

0 Kudos
3 Replies

984 Views
stanish
NXP Employee
NXP Employee

Hello,

Attached is the Special Edition License file for CW HC08 v6.x

If I remember correctly it should include unlimited assembler. C object code limited to 64kB. Not sure about the linker.

Hope it helps.

Stan

0 Kudos

1,129 Views
Mag2023
Contributor I

Can't understand the logic behind this, CW6.3 is no longer supported, it runs on 32 bit OS still customer wants to stick Motorola, Freescale and now NXP with good experienced with CW6.3 still it is not free.  

0 Kudos

1,785 Views
vicentegomez
NXP TechSupport
NXP TechSupport

 Sorry no

 

and also be aware that codewarrior 6.3 is no longer supported, it only runs on 32 bit OS.

0 Kudos