Is it possible to change the firmware of CodeWarrior USB TAP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to change the firmware of CodeWarrior USB TAP?

Jump to solution
904 Views
petkotabakov
Contributor I

Is it possible to reprogram the firmware of CWH-UTP-ONCE-HE CodeWarrior USB TAP (for ONCE DSC) with firmware for
ColdFire (CWH-UTP-CF-HE)? I believe the hardware is the same, only a cross connector for BDM is needed. The problem
is that USB TAP for ColdFire is discontinued, and only the model for ONCE DSC is available on the market. CodeWarrior v7.1

Labels (1)
0 Kudos
Reply
1 Solution
718 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

No. It's not possible to reprogram CWH-UTP-ONCE-HE to support Coldfire.

to work with Coldfire, please use either of the below emulator tool:

USB ColdFire Multlink|NXP 

Universal Multilink Development Interface|NXP 

Universal Multilink FX High-Speed Development Interface|NXP 

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
719 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

No. It's not possible to reprogram CWH-UTP-ONCE-HE to support Coldfire.

to work with Coldfire, please use either of the below emulator tool:

USB ColdFire Multlink|NXP 

Universal Multilink Development Interface|NXP 

Universal Multilink FX High-Speed Development Interface|NXP 

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply