Is it possible to change the firmware of CodeWarrior USB TAP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to change the firmware of CodeWarrior USB TAP?

跳至解决方案
957 次查看
petkotabakov
Contributor I

Is it possible to reprogram the firmware of CWH-UTP-ONCE-HE CodeWarrior USB TAP (for ONCE DSC) with firmware for
ColdFire (CWH-UTP-CF-HE)? I believe the hardware is the same, only a cross connector for BDM is needed. The problem
is that USB TAP for ColdFire is discontinued, and only the model for ONCE DSC is available on the market. CodeWarrior v7.1

标签 (1)
0 项奖励
回复
1 解答
771 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

No. It's not possible to reprogram CWH-UTP-ONCE-HE to support Coldfire.

to work with Coldfire, please use either of the below emulator tool:

USB ColdFire Multlink|NXP 

Universal Multilink Development Interface|NXP 

Universal Multilink FX High-Speed Development Interface|NXP 

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
772 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

No. It's not possible to reprogram CWH-UTP-ONCE-HE to support Coldfire.

to work with Coldfire, please use either of the below emulator tool:

USB ColdFire Multlink|NXP 

Universal Multilink Development Interface|NXP 

Universal Multilink FX High-Speed Development Interface|NXP 

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复