How to let the Multilink Universal Rev.C work under CW7.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to let the Multilink Universal Rev.C work under CW7.1?

2,183 Views
lisuoyu
Contributor I

Chip is McF52259 , Simulator is the Multilink Universal rev C, Development environment using CW7.1. why can't download the program?

Labels (1)
0 Kudos
Reply
2 Replies

1,880 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi souyu,

in order to use Multilink Universal rev C working with McF52259 and CW7.1.

we  need:

1. download and install USB Multilink Universal Resource CD  . it incl&E multilink universal firmware update utility.

P&E Microcomputer Systems - USB Multilink Universal - USB Multilink Universal All-In-One Development...

2. connect Multilink Universal rev C with computer USB port. then follow attached video to update multilink firmware for CF v2-v4.

then you can use Multilink Universal rev C working with McF52259 and CW7.1

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,880 Views
takaoyamada
Contributor IV

Greetings,

I would also like to add the use of the Codewarrior patch I have created to get the latest hardware working on the classic Codewarrior:
P&E Microcomputer Systems

Takao Yamada

P&E Microcomputer Systems

0 Kudos
Reply