I use CW8.2 for DSC. And there is no *.o files when I build the project. Now I need to get O files of my project.
I tried to seek in User Manuals, but haven't found.
If there is anyone out there know how to set the CW to generate the O files?
Thanks!
P.S. :If I build a new project "TEST", there will generate a folder "ObjectCode" in path “{Project}\TEST\TEST_Data\sdm_external_memory”, but it is empty, I don't know if it is the same problem as mine.
解決済! 解決策の投稿を見る。
Hi,
I recall a CodeWarrior Classic supported a pragma
#pragma store_object_files on
Hope it help.
Stan
Hi,
I recall a CodeWarrior Classic supported a pragma
#pragma store_object_files on
Hope it help.
Stan
Thank you very much, Stanislav! A friend told me the same method as yours yesterday, and that really help.
Hello Freeman
There's no option in Classic CodeWarrior v8.3 for 56800/E to generate the object files.
The command-line compiler can generate separate object files, the option for this switch is '-codegen'. But this is not available for the compiler plugin in CodeWarrior IDE. Such behavior is same with CodeWarrior for MPC56xx as well.
The new CodeWarrior v10.x for MCU also supports 56800E products. The compiler plugin in this IDE can generate separate object files.
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
Hope it helps!
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Xin! So I try another way that recall
#pragma store_object_files on
Freeman