How to convert GIF to HEX formatted so 52259 can display image as a web server

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to convert GIF to HEX formatted so 52259 can display image as a web server

2,638件の閲覧回数
Kratz
Contributor IV

I need to know how to convert GIF to HEX formatted so 52259 can display image as a web server.

 

The example software that came with it has this kind of hex image file structure.

 

          static const unsigned char data_header_gif[] = {
          /* /header.gif */
          0x47, 0x49, 0x46, 0x38, 0x39, 0x61, 0xde, 0x03, 0x32, 00,
          0xb3, 00, 00, 0x99, 0x98, 0x98, 0xf9, 0xf7, 0xf6, 0xc4,
          0xca, 0xcb, 0x62, 0x60, 0x60, 0xf6, 0x98, 0x69, 0x20, 0x1c,

         ect. . .

I found a free program that can convert a GIF file to a hex file, but it lists the hex in one long sting of numbers like below:

 

         64F0B245AE48A2DD67301A4437C60809C651EA862A3BF31D3584B5225C0E32F26A   ect. . .  and nearly to infinity.

 

What ways are available to convert from the GIF file to a formatted HEX file?

 

Thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,828件の閲覧回数
Lundin
Senior Contributor IV

>   64F0B245AE48A2DD67301A4437C60809C651EA862A3BF31D3584B5225C0E32F26A

 

Why can't  you write a simple parser of that hex chunk yourself then? You should be able to do it in less than 30 minutes.

0 件の賞賛
返信

1,828件の閲覧回数
J2MEJediMaster
Specialist I

I did not have much luck finding a GIF convertor. There are a lot of BMP-to-hex convetors, though. It should be easy enough to use any paint program to change the GIF to a BMP. This link has the source code for BMP to hex, so you can modify the program to generate the output the way you need it.

0 件の賞賛
返信