How to combine assembly code with C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to combine assembly code with C

11,907 次查看
Jalen
Contributor I
I am new to code warrior and embedded design. How do i combine C code with assembly codes? Thx
标签 (1)
0 项奖励
回复
4 回复数

1,813 次查看
bigmac
Specialist III
Hello and welcome to the forum.
 
You can incorporate assembly instructions directly within a C function, using "inline assembly".  You should find further information within the manual for the compiler.  The format for some of the instructions will differ from that for "standard" assembler.
 
Alternatively, you could create a separate file, written in "standard" (relocatable) assembler, and consisting of assembly sub-routines.  However, parameter passing to these routines will need to match the requirements of C for the MCU you are using, and a prototype for each routine will need to be visible from the C module(s).  Perhaps the simplest method of handling parameters for the assembly routines is via global variables.
 
Regards,
Mac
 
0 项奖励
回复

1,813 次查看
Alban
Senior Contributor II
Hello,

The post referenced after is showing how to do INLINE assembly.
You create a asm{} and put your assembly code in the curly brackets:
/message?board.id=CFCOMM&message.id=235 http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=235" target="_blank
Look for "asm {" as a keyword in the search at the bottom of forum pages.

Cheers,
Alban.
0 项奖励
回复

1,813 次查看
CrasyCat
Specialist III
Hello
 
Just to close the loop here, the HC08 or HC12 assembler manual include a section around mixing C and assembly in an application.
 
  - Depending on the CPU you are using open the file {Install}\Help\PDF\Assembler_HC08.pdf or
    {Install}\Help\PDF\Assembler_HC12.pdf.
  - For HC08 go to chapter "Using the HC(S)08 Assembler", section
     "Mixed C and Assembler application"
  - For HC12 go to chapter "Using the HC(S)12 Assembler", section
     "Mixed C and Assembler application".
 
 
CrasyCat
0 项奖励
回复

1,813 次查看
Jalen
Contributor I
Thanks loads to everyone for your help!
0 项奖励
回复