How can I flash my application?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I flash my application?

725 Views
UB39
Contributor I

Hello!

 

I write my application and tested it inside internal RAM. Now I wanna flash it to use it as a stand alone application.

 

Therefore I changed the debug configuration from MK60N512VMD100_INTERNAL_RAM to MK60N512VMD100_INTERNAL_FLASH, but it has no effect.

With the internal Flash configuration I can debug my program as before. But after a reset or after power up my application doesn t run.

 

Using the flash might be more complicated than I expect.

So what must I do to get my program into flash?

 

I also try to use the simple flash programmer that is part of Codewarrior, but I alway get error messages when I try to use it.

 

I use the TWR K60 Tower and CodeWarrior 10.1

 

May Thanks

 

Ulf

Labels (1)
0 Kudos
Reply
1 Reply

588 Views
J2MEJediMaster
Specialist I

Please do not cross post your question into other forums. I have answered it elswhere.

 

---Tom

0 Kudos
Reply