GNU Configure Problems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GNU Configure Problems

2,329 次查看
glowkeeper
Contributor I
Hi,
 
I'm having a problem using the MetroWerks CodeWarrior command line compiler under cygwin when trying to build an open source package for the Wii using gnu's configure, make, make install scenario.
 
Basically, no matter what options I give, when I run configure, I get this far: 
 
configure: error: C preprocessor "mwcceppc.exe" fails sanity check
I realise this is a long shot, but has anyone ever come across this before? If so, could you shed some light on the problem?
 
Glowy
 
ps.  mwcceppc.exe -version    
Metrowerks C/C++ Compiler for Embedded PowerPC.
Copyright (c) 2006, Freescale Semiconductor, Inc.
All rights reserved.
Version 4.1 build 60831
Runtime Built: Aug 31 2006 18:18:06
标签 (1)
0 项奖励
回复
2 回复数

759 次查看
LeoAtreides
Contributor I
Hi there,
 
 
  I have had similar problems trying to get software packages to ./configure . Did you figure out how to do this, and if so can you let me know how this is done
 
regards
 
Leo
0 项奖励
回复

759 次查看
J2MEJediMaster
Specialist I
"Fails sanity check" is a new one on me. Nor does it sound healthy.

I'd recommend that you submit a service request on that. Click here to file a service request.

---Tom

0 项奖励
回复