FreeMaster recorder with MC56F8006DEMO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeMaster recorder with MC56F8006DEMO

Jump to solution
2,469 Views
Gibson
Contributor II

Hi,

 

I'm trying to use the FreeMaster's recorder with the MC56F8006DEMO. As I tried to activate a record window in FreeMaster, I'm getting error message : the hardware recorder could not be initialized (Invalid size specified). I changed the Data buffer size, Recorder buffer length and now I have a size incompatible with bus width error.

 

Is there a guide to properly size the "Data buffer size", "Recorder buffer length", "Command buffer length" in the initialization of the PC_Master Bean?

 

Thanks,

 

Gibson

Labels (1)
Tags (1)
0 Kudos
1 Solution
741 Views
Gibson
Contributor II

Hi Tom,

 

I already check most of the thread for Freemaster. No much on the freemaster's recorder.

 

Anyway, by trial and error, I finally find some working settings.

 

In my case with the MC56F8006DEMO:

 

- Data buffer size : 40

- Recorder buffer length : 80

- Command buffer length : 4

 

Regards,

 

Gibson

View solution in original post

0 Kudos
3 Replies
741 Views
believe
Contributor I

I haveing use Freemaster do BLDC project, it can do  properly, but I can not find  "Data buffer size", "Recorder buffer length", "Command buffer length" , where they are?

 

Are you Chinese? I am doing sensorless BLDC with MC56F8006,can we communication with 8006?

My mobile phone is :+86 13705541506,my QQ is 356119619,can we study with each other?

0 Kudos
741 Views
J2MEJediMaster
Specialist I

You might try the using the search function to search the forums. I entered "Freemaster" and got a few hits. This https://community.freescale.com/message/45605#45605 looks the most promising. Hope it helps.

 

---Tom

0 Kudos
742 Views
Gibson
Contributor II

Hi Tom,

 

I already check most of the thread for Freemaster. No much on the freemaster's recorder.

 

Anyway, by trial and error, I finally find some working settings.

 

In my case with the MC56F8006DEMO:

 

- Data buffer size : 40

- Recorder buffer length : 80

- Command buffer length : 4

 

Regards,

 

Gibson

0 Kudos